Part Number: CC2533 Other Parts Discussed in Thread: REMOTI Dears,
I have some question about to apply CC2533 in RF4CE Receiver.
When CC2533 is applied to RF4CE Receiver, is there a recommendation about external flash memory size?
Do you have…
Part Number: CC2530 Other Parts Discussed in Thread: CC2533 , Dear champs,
My customer uses CC2533 in an existing product today, but looking to use CC2530 in some products. How compatible are these?
Pinouts are very similar apart from pins 1-4 which…
Part Number: CC2533 Hi, support team
My customer has the questions as follow:
I found the code is 64K flash of RemoTI-CC253x. But my chip is cc2533F32. How can I find the right SDk for cc2533F32 RF4CE? How to find the cc2533F32 RF4CE source code which…
Part Number: CC2533 Hi TI CC expert,
We are using CC2533 for a long time.
This time, due to the program's function deletion, the wireless function is not needed, and I don't want to change the chip, so I will use this device directly.
Then the question…
I setup NPI server at windows PC IP=192.168.1.122, and Mass production tool at windows PC IP=192.168.1.222. and connection between NPI server and Mass poroduction tool
I could capture the data send from NPI server to Mass poroduction tool , and the…
Part Number: CC2533 Hi Team,
A customer has been testing battery monitor with CC2533 for a while, and he met some problem.
He uses our example code [as follows]. The value to monitor is 2.146v, it can be monitored if use a regulated source to jump…
Part Number: CC2533 We have a specific 2534 dump file which can not work with their new application correctly with RF signal lost isseue with distance 1meter.
I attached the NV ram parser files and hex file to Ti. Please help have TI's RD to analyze…
Part Number: CC2533 Other Parts Discussed in Thread: REMOTI
Tool/software: Linux
Hi Support,
if we want to reset the Configuration parameter and status attribute to the FW default value from the RemoTI apl.
RTI_WriteItem, StartupOption=2)
Please…
Part Number: CC2533 Hello,
I’m working on ir learning with cc2533. But I don’t succed in capturing anything …
My IR_IN is on Port 1 pin 0.
Here is my initialization code :
“
void initIR_Reception(void)
{
// Peripheral I/O control
PERCFG…