Koichiro-san,
Koichiro Tashiro said: It seems iPhone supports SBC and AAC, android supports SBC and aptX. And iPhone first tries to use AAC, then if it fails, it switches to SBC.
According to A2DP profile specifications, both source and sink are supposed…
Part Number: CC2564MODA Other Parts Discussed in Thread: CC256XM4BTBLESW , CC2564 Does the Module have a default stack programmed in?
If so, what is the Profile it defaults to?
IF I download the CC256XM4BTBLESW: TI dual-mode Bluetooth stack on TM4C MCUs…
Part Number: CC2564MODNEM Other Parts Discussed in Thread: CC256XM4BTBLESW , CC2564 Tool/software: Code Composer Studio Hello
I'm evaluating Bluetooth transmission on kit EK-TM4c12954XL and CC2564MODNEM, using Bluetopia 1.2-R2 obtained from CC256XM4BTBLESW…
Part Number: CC2564MODA Other Parts Discussed in Thread: CC2564 , CC3200AUDBOOST Hi, My customer is implementing A2DP with below HW+SW. HW: DK-TM4C129X + CC2564MODA SW: www.ti.com/.../CC256XM4BTBLESW Customer changed the A2DP demo so that single SSI (SPI…
Part Number: CC2564MODA Hi, My customer is implementing A2DP with below HW+SW. HW: DK-TM4C129X + CC2564MODA SW: www.ti.com/.../CC256XM4BTBLESW Customer changed the A2DP demo so that single SSI (SPI master mode) is used to send the data. (LRCLK is generated…
Hi Vihang,
Could you please help me what is the basic changes in CC256XM4BTBLESW Sample Applications, when i am using board EK-TM4C1294XL in place of
DK-TM4C129X .
I am trying to run the SSP Demo as of now. Attached a snapshot…
Part Number: CC256XB-BT-SP We develope an USB Stick to connect some Bluetooth devices from us (with the same stack and the same Hardware).
Now it is on the market and some of our customers sometimes have problems opening the ports.
The function SPP_Open_Remote_Port…
Part Number: CC256XB-BT-SP Other Parts Discussed in Thread: TM4C123GE6PZ Dear support team
We develope an USB Stick to connect some Bluetooth devices. I connect the devices over SPP_Open_Remote_Port.
I want to change the timout of the port open.
I use…
Hi Dawid,
I was able to get the dual-mode BT and BLE sample applications (like the SPPLEDemo) to work out-of-the-box on the DK-TM4C123G and CC256XQFNEM boards using the CC256XM4BTBLESW SDK. I was also able to detect the SPPLE custom service from BLEScanner…
Other Parts Discussed in Thread: CC256XQFNEM , CC256XM4BTBLESW , CC2564MODAEM Hi everyone,
I want to know how to run the SPPDEMO with DK-TM4C129X & CC2564B EM.
I always get the following error with or without "#define __SUPPORT_CC256XB_PATCH__" in BTPSVEND…