Part Number: CC256XQFNEM Hi all,
I tried HFP Demo but I cannot get any audio at btoh sides. Here is my setup:
Hardware: CC256XQFNEM + CC256XEM-STADAPT + STM32F4DISCOVERY
Software: STM32 Bluetopia SDK, IAR Embedded Workbench for ARM v7.50.2.10505
Story…
Other Parts Discussed in Thread: CC256XQFNEM , CC2564 Hi everybody,
I need help to configure the i2s interface between the two eval boards CC256xQFNEM and TLV320AIC3100EVM-U.
To configure TLV Codec i set the registers using i2c in a way that is ok using…
Part Number: CC2564 Other Parts Discussed in Thread: CC256XQFNEM , , The CC256x Wiki mentions a code CC256xQFNEM as required hardware. And it has a link that points to a non-existing TI page.
Just to be on the safe side, is that module the same as CC2564MODNEM…
Other Parts Discussed in Thread: CC256XQFNEM , CC2564 , BOOST-CC2564MODA Hi, I want to do quick evaluation with bluetooth stuff and I got interrested in CC256XQFNEM board. Because I do not have any of experimenter boards mentioned on page of CC256XQFNEM,…
Other Parts Discussed in Thread: CC256XQFNEM , CC2564MODNEM , CC2564MODA , CC2564MODN , CC2564MODAEM , CC256XSTBTBLESW I want to start to develop the Dual Model bluetooth which base on STM32F4 ,and now i have a STM32F407 EM ,So Do i have to buy a STM32F4 Discovery…
Other Parts Discussed in Thread: CC256XSTBTBLESW Hi Everybody,
i need help!
I have connected DISC1 and QFNEM directly, without ADAPT board. I would like to know the correct procedure to port BLUETOPIA Examples to DISCOVERY board.
They are developed for…
Other Parts Discussed in Thread: CC256XQFNEM , CC2564 Hi all,
I need your help!
I have my Discovery connected directly to CC256XQFNEM board. I'm running HFPXDemo from Bluetopia 4.0.2.2 SDK.
The connection in made directly to PD8 and PD9 pins. (HCI_UART…
Other Parts Discussed in Thread: CC256XQFNEM Hi, I have this problem:
I initialize HCI_DriverInformation with the following line:
HCI_DRIVER_SET_COMM_INFORMATION(&HCI_DriverInformation, 1, VENDOR_BAUD_RATE, cpUART);
in order to open the BT stack wi…
Other Parts Discussed in Thread: CC256XQFNEM , CC256XB-BT-SP Hi everyone,
I want to know how to download patch.
Now I have followed the process to download patch.
HW : DK-TM4C129X + CC256XQFNEM SW : BHET, CCSv6.1
1.Convert the Service pack (CC2564B SP 1…
Other Parts Discussed in Thread: CC256XQFNEM Hi,
I'm using STS32F4-DISC, cc256xQFNEM and TLV320AIC3100EVM-U with assisted mode.
I'm trying to connect two systems using HFP protocol and running HFPDemo HFPAGDemo (bluetopia version 4.0.2.2).
There is…