Good morning Ryan,
No, the same type of sensor. I made some changes in the code and now I can connect with more than one sensor.
Thank you very much for your help.
Cristiane Bellenzier Piaia
Hi Alex,
I got some feedback from the Hardware apps team.
I is possible to run multiple spi Intefaces for the Coexistence feature if you activate the chip select pin and toggle it when communicating.
Regards,
Alex
Part Number: CC2652RSIP Hello, we are developing a product with the cc2652rsip that can be updated wirelessly with the OAD protocol and an external flash memory, however after some tests and integrations we have the following questions:
About the factory…
Part Number: CC2652RSIP Hi team,
I have a need to check the operational status of the specified timer (stopped, running medium).
Look at Timer's API and feel that Timer_control may be able to do this. However, it is only seen in the Timer.h file as stating…
Part Number: CC2652RSIP Other Parts Discussed in Thread: SIMPLELINK-CC13XX-CC26XX-SDK With ZStack I'm trying to send custom temperature report triggered by timer.
I started from zed_temperaturesensor example, added the timer (which successfully triggers…
Part Number: CC2652RSIP Other Parts Discussed in Thread: ENERGYTRACE ,
Hi, I am working with CC2652R1F with a simple peripheral example.
In a modified exercise , I tried to achieve the standby power claimed in datasheet ( www.ti.com/.../swrs207h.pdf - –…
Part Number: CC2652RSIP Hello,
Could you provide any information of wired (UART, I2C) and over-the-air upgrade (OTA)? What applications should be used for the OTA?
Thanks,
Alex
Part Number: CC2652PSIP Other Parts Discussed in Thread: CC2652RSIP , Hello,
What are differences between projects created for CC2652RSIP and CC2652PSIP? Are they functionally identical? Can be used project, created for CC2652RSIP, for the new wireless MCU…
Part Number: CC2652RSIP Other Parts Discussed in Thread: SYSCONFIG , Hi! Using the SimpleLink BLE stack, I'm trying to run the "simple peripheral with offchip OAD" example and running into problems. The OAD master is giving me an "attribute write error…
Part Number: CC2652RSIP Hello
I am trying to make a program with "Differential phase-shift keying (D-PSK)" by 1Mbps on CC2652RSIP.
But ,according to the data seet, we can use (G)FSK, MSK and OOK.
Can I use D-PSK by 1Mbps? a nd How do I use it…