Part Number: CD40109B Other Parts Discussed in Thread: UCC44273 , UCC27517 , TXH0137D-Q1 , CD4504B , TXH0137D ,
This is reg translating a 3.3 V PWM Signal to +15 V levels with approx 5 mA Source & Sink
CD4504 Data Sheet is not guaranteeing this translation…
The CD40109B-Q1 datasheet says:
Thereare no restrictions on the sequence of application of V DD , V CC , or the input signals.
The CD4010B-Q1 datasheet does not mention anything similar, and shows in the schematic diagram on p. 2 that there are diodes from…
Part Number: CD4044B Other Parts Discussed in Thread: CD40109B Hi
We are using CD4044B chips connected to 15Vcc. Therefore, the latched outputs signals(Q1,Q2,Q3 and Q4 of the chips) of the chips will be at 15V. What would be the best solution to translate…
Part Number: CD4051B-Q1 Other Parts Discussed in Thread: CD40109B-Q1 Hi,
I'm interested in using the CD4051BQPWRQ1 and wondering what signal level the select lines should be at for VDD = 15V? Analog input signals would be in the 0 to +10V range.
Thank…
Other Parts Discussed in Thread: ISO7710 , ISO7041 , ISO7021 , SN74LVC2G17-Q1 , ISO7731-Q1 , ISO7742-Q1 , SN74LVC1T45-Q1 , CD40109B-Q1 , ISO7742 , CD40109B , ISO122 , ISO224 Hi TI Team,
I wanted to Isolate ADC input pins which is coming from external circuitry, Its…
Part Number: LM321 Other Parts Discussed in Thread: MC33063A , TLV1805-Q1 , TLV1805 , L293D , DS3668 , CD40109B-Q1 Hi,
I need to design a circuit for generating 20 volts output from a 3.3 volt positive signal .My board has only 12v and 15 volt supplies.
…
Part Number: CD4503B Other Parts Discussed in Thread: CD40109B Hi Friends. I have a small doubt. If the VDD pin is connected to +12V , is it possible to switch the output Q1 by providing 0 and +3.3V at the input D1
In the circuit given I am using the buffer…
Part Number: SN74AXC8T245 Other Parts Discussed in Thread: SN74LVC8T245 , , SN74LVC2T45 , SN74LVC16T245 , LSF0108-Q1 , TXB0108 , LSF0108 , SN74LV4T125 , CD40109B Hey Guys,
I made a terrible mistake: I use the SN74AXC8T245PW in my design and reconfigured the VccB…