Part Number: CD4066B
Hi, previously, I was using MAX14866 SPI controlled high voltage SPST analog switch.
This was nice but it was too expensive and it had excessive channels.
So I want to change to TI's SPST analog switch solution. Can I get a recommendation…
Part Number: CD4066B Switch is to be used in circuit for analog integration of AC signal. (range of 0,3Vpp to 1,5Vpp (see below picture).
First, we invert input signal. Then we create positive (rectified) input voltage with usage of S1 and S2 which switches…
Part Number: CD4066B Other Parts Discussed in Thread: TMUX6112 E2E,
I have a problem when they are testing CD4066. It seems the control voltage will also need to be negative if CD4066 is powered by +/-5V supply, and that is not described in the datasheet…
Part Number: CD4066B Hello team,
for CD4066BM96. What is the difference between the E4 and G4.
CD4066BM96G4
CD4066BM96E4
Thank you for your support!
Errol Leon
Texas Instruments
Field Application Engineer
Christian,
Placing 2V on SIG_A_IN with VDD = 0V violates the absolute maximum ratings in the datasheet.
The 2V on the SIG_A_IN will bias the internal protection diode and you will see leakage current to Vdd. This current could also backpower the gate…
Shu-Cheng,
The CD4066 is correctly powered with 7.5 V on VDD and -7.5 on Vss.
If your signal passing through the switch is +/-6V you will have better Ron if your supply rails are greater than +/-6V
The function table is a little strange but it is communicating…
Part Number: CD4066B Other Parts Discussed in Thread: CD54HC4316
Hi Team,
The customer is using CD4066B.
There are 4 files in the attachment. The customer uses 2 different amplitudes of the input signal with a fixed frequency=5KHz with the control input…
Part Number: CD4066B Other Parts Discussed in Thread: CD4051B , MPC508 I'm designing an 8:1 standard-definition NTSC video multiplexer using 2x CD4066B. Video sources are small cameras that operate on a single 3.3 to 5V rail.
At paragraph 3 on pg 1…
Part Number: CD4066B Other Parts Discussed in Thread: SN74HC4066 Hi
I have a question about this device. Is that possible to add any capacitor to IN or OUT line?
If it is possible, how much is that we can add?
I saw some specification such as input capacitor…