Part Number: CD4503B Other Parts Discussed in Thread: TINA-TI Hi there,
I am looking for an IBIS model for the CD4503B. I see there is SPICE model available on the products page, however, when I try to implement the model, I get the error:
ERROR…
Hi Emrys Maier, Thank You for your reply.
In the datasheet of CD4503B , it is clearly written the input voltage at any input pin is -0.5V to VDD +0.5V.
Still, I have a doubt whether 3.3V is sufficient enough to switch the 12V output.
Part Number: CD4503B Dear, support team. Safety-Related Certifications: IEC 62368-1 Can you please provide us with this certification report & certificate for the CD4503B ? Do we have such a report for the CD4503B?
Best Regards, Hiroaki Yuyama
Part Number: CD4503B Other Parts Discussed in Thread: SN74AXC8T245 Hi team,
My customer needs some buffer and the requirement as below, could you please help to recommend BU's hero product?
Thanks!
1. more than 4 channel, single direction, signal…
Part Number: CD4503B Other Parts Discussed in Thread: CD74HC4511 With a 5V supply and 2V across the LED (thus 3V across the driver), am I correct in assuming that if I were to connect a LED from the CD4503B output and ground the output resistance of the…
Hi Max,
I don't really think having two terminators in parallel would happen in this configuration since CD4503B is a 2-way switch.
I've changed my drawing a bit so it might seem clearer to you.
Full+Half Duplex Configuration_Remove mux.pdf
…
Hello,
A suitable high voltage buffer would be the CD4010B or the CD4050B. The CD4503B has three state outputs if those are required.
Please note that we are trying to ensure that all posts are answered. With any new posts, we will be sure answer…
Part Number: SN54HC367 Other Parts Discussed in Thread: SN74HC367 , SN74HC373 , CD54HC367 , CD4503B-MIL Hi Team,
A customer is looking for an equivalent device to National Semiconductor's MM70C97J/883. Upon checking our list of tri-state hex buffers…
Other Parts Discussed in Thread: CD4503B , CD4049UB Hello all, I've been working off of TI "Ultrasonic Distance Measurement With the MSP430" application report (http://www.ti.com/lit/an/slaa136a/slaa136a.pdf) and I found that I was having a bit of difficulty…