Part Number: CD74HC4053 Other Parts Discussed in Thread: TMUX4053 Hello,
On ti.com, the CD74HC4053M96 lead finish / ball material is listed as 'NIPDAU | SN'. Is it possible to only order this P/N with only the NIPDAU finish, not SN?
Thanks,
Ste…
Part Number: TMUX4053 Other Parts Discussed in Thread: CD74HCT4053 , CD74HC4053 Hi team,
We are choosing SPDT MUX device for xxx4053xxx.
Question1: What's the performance difference of prefix between TMUX4053 and CD4053?
We could see they have…
Part Number: CD74HC4053 HI
1. What is the VCC, VEE supply current in the worst case?
The design conditions are as follows.
VCC: +5V
VEE: -5V
Frequency: 1Mbps
2. Is there any difference between single power supply mode (VCC:+5V, VEE:GND…
Part Number: TMUX4053 E2E,
I saw that there are new TMUX4053 devices and wanted to know if they are similar to the other 4053? What is the difference between these devices?
Thank you,
Adam
Part Number: CD74HC4053 Hi team
Could you help to check what is the output status of CD74HC4053 when the device is disabled(When EN is High), is it tri-state status?
Part Number: CD74HC4053 Other Parts Discussed in Thread: TMUX1574 The recommended operating condition for the following parts: The TI 74HC4053 Vcc - GND is 2 volts to 6 volts. For the Nexperia 74HC4053 Vcc - GND is 2 volts to 10 volts. I had though that…
Part Number: CD74HC4053 Hi, Is it OK to float if not used with the following pins? ・ A: B: C [0-1] IN/OUT pin ・ COM A: B OUT/IN pin Best regards, Yuto Sakai
Other Parts Discussed in Thread: CD74HC4053 Hi Team,
The customer would like to test the reliability of their circuit for CD74HC4053 . He needs to get the number of internal logic gates and the number of
internal transistors for CD74HC4053.
Can…