Other Parts Discussed in Thread: CDC351 , CDC3RL02 , CDCLVP1102 , CDCLVP2102 , CDCLVC1102 Hi ,
May I know TI have any clock buffer (distributor) 1:2 with tri state output.
Supply Min is 1.8V
Regards
Hari
Other Parts Discussed in Thread: CDCLVC1102 , CDCLVP1102 , CDC3RL02 Could suggest a solutoin use on 24MHz clock buffer use on AR glasses?
We want to redriver 24MHz camera clock because the clock trace is too long:
CPU 24MHz CLOCK --> 1.5m Coax cable(50ohm…
Part Number: LMH2191 Other Parts Discussed in Thread: CDC3RL02 Hi,
I have a few questions about the LMH2191.
Q1.I want to input an external reference signal to the LMH 2191 and output a square wave. Input : 10MHz,Sine wave Output: 10MHz,Square wa…
Sorry. CDC3RL02 does not meet the phase noise spec.
It has "–149 dBc/Hz at 10-kHz Offset Phase Noise".
But my Rubidium clock has " <–155 dBc/Hz (10 kHz) " .
Phase noise (SSB) <–130 dBc/Hz (10 Hz) <–140 dBc…
Hi Céline,
The LMH2191 buffer does not belong to the Clock and timing group. However, from reading the datasheet ( http://www.ti.com/lit/ds/symlink/lmh2191.pdf ), Page 12, it appears that the AC input impedance can be as low as 10 KOhm for a 1Vpp…
Other Parts Discussed in Thread: CDC3RL02 , CDC3S04 Dear,
Our customer has been using Rubidium clock with this phase noise and 10MHz/1.41Vp-p/50ohm sine wave output..
And looking for proper square wave converter for the clock to make 10MHz square /2…
Other Parts Discussed in Thread: LMV112 , CDC3RL02 , CDCLVC1102 , LMK00804B , LMK00105 Hello,
Can LMV112 Clock Buffer be used with CMOS Oscillator (like DSC1003)?
Thank you,
GMC
Other Parts Discussed in Thread: CDC3RL02 , CDC3S04 , LMV7219 , LMH7322 , LMH7220 Hi Team,
Our customer is looking for a sin wave clock buffer for 1k to 10kHz sin wave input.
Which part would best match for this requirement ?
I found the following devices…