Part Number: CDCDB800 Hello E2E,
I’m looking to use CDCDB800RSLR LP-HCSL 1:8 clock buffers to provide 100MHz PCIe reference clocks across a system. The datasheet for this component mentions that it expects an LP-HCSL input clock, but in our case…
Part Number: CDCDB800 Dear Team,
May you give some substitute solution for me to replace IDT?
9SQL4954CNLGI<-> CDCDB400
9ZXL0651EKILFT<-> CDCDB800
Thanks a lot.
Jimmy
Part Number: CDCDB800 Other Parts Discussed in Thread: CDCDB803 Hi Team,
Customer is consulting the detailed size of thermal pad. Pls help us here because our D/S doesn't contain it.
Best,
Stanley
Part Number: CDCDB800 Dear team,
I want to use TICSPRO to fine-tune register value of CDCDB800.
Refer to device EVM user guide, there should be CDCDB800 module in TICSPRO> Select Device → Clock Distribution with Divider → CDCDB800.
I only…
Part Number: CDCDB800 Hi Team,
Does our CDCDB800 fully P2P with 9ZXL0851EKILFT? Customer needs one can replace 9ZXL0851EKILFT in their board directly. Pls help us here. Thanks.
Best,
Stanley.
Part Number: CDCDB800 Hello team,
I would like to confirm meaning of Toe and Tod spec of CDCDB800.
Datasheet p.8, these are specified as maximum 10 CLKIN Periods. Does this mean in case CLKIN_P/CLKIN_N is 100MHz, it will take maximum 100ns(10ns x 10 periods…
Part Number: DS320PR1601 Other Parts Discussed in Thread: CDCDB800 Hi,
1 a)If we use SM bus for programming the redriver(DS320PR1601) instead of EEPROM, where will be the data saved?
b)Don't we need to program every time we turn on the add in card…
Thank you, Asim.
You may also wish to check the datasheet for CDCDB800 and CDCDB400 as they also have the same statement in the pin configuration section for CKPWRGD_PD#. "If unused, the pin can be left no connect."
Thanks Connor
Do you have any data you can share for the expected swing with a 60MHz clock, close to max recommended VCC with standard termination?
If we do not already have this data could someone measure it on an EVM?
Could someone also provide similar…
Part Number: LMK1C1106 Other Parts Discussed in Thread: CDCDB800 Hi team,
Can you help recommend the P2P alternative of 9DBV0641AKILFT?
Renesas-9DBV0641.pdf
Thanks
Lillian