Part Number: CDCE6214-Q1EVM Hello Team,
may I kindly ask you for the BOM, especially the PN of the 25MHz crystal, please.
Also, how can I calculate the values of the integrated loop filter to achieve lowest loop bandwidth of 100kHz?
Thanks and Best…
Part Number: CDCE6214-Q1EVM Hi Team,
We are using TICS Pro + CDCE6214-Q1EVM for testing. And we have some questions.
1. If we set OUT1 = LVDS 150MHz clk and set 25MHz PFD, 0.25%. How should I calculate spread frequency?
2. When I change output…
Part Number: CDCE6214-Q1EVM Hi there,
I just started playing around with the eval board and the bias current and load capacitance settings do not make sense to me.
Could somebody provide the datasheet or information on the 25 MHz Xtal used on the…
Part Number: CDCE6214-Q1 Other Parts Discussed in Thread: , CDCE6214 , LMK03318 We are evaluating CDCE6214-Q1 on the CDCE6214-Q1EVM evaluation kit.
To assure correct operation we would like to simulate the loop filter in Plladium, however the part is…
Part Number: SN75LVDS387 Other Parts Discussed in Thread: CDCE6214-Q1EVM , SN65LVDS2 , SN65LVDS4 , DS90LVRA2 , SN75LVDS386 Tool/software: Hi team,
Is the related post/question still true? ( https://e2e.ti.com/support/interface-group/interface/f/interface…
Part Number: CDCE6214 Hi guys,
I'm bringing up a new design where the CDCE6214 is programmed over USB. The Microchip MCP2221A acts as an USB-I2C bridge.
We have a CDCE6214-Q1EVM dev kit that can be used to validate output signals and generate…
Yufeng,
EEPROM programming is a must if the clocks are required at startup for application operation. If potentially incorrect clocks is not an issue at startup, then the SOC can configure registers after power-on. If the latter is the case, my recommendation…
Liu,
I have attached the two configuration files here. Please let me know if a larger swing is required, and we can change the output format from LP-HCSL to LVDS.
CDCE6214_24MHz_In_144MHz_Out.tcs
CDCE6214_24MHz_In_74p25MHz_Out.tcs
For the schematic…
Part Number: CDCE6214-Q1 What is the difference between CDCE6214-Q1 and CDCE6214-Q1EVM?
Also, I am interested to know the tech node of this part and its sourcing. Is it readily available in production volumes?
Where are its wafers produced and where…
Hello ren,
The GUI can be found on TICSPRO-SW. I do not think we have an EVM for the commercial device however there is a CDCE6214-Q1EVM (automotive). Are you using the CDCE6214-Q1EVM?
The USB2ANY tool can be used to support different communication…