Hi Dice-K,
The pin configuration of these devices is identical to CDCLVC1102 and CDCLVC1103:
We will update the pin configuration of LMK1C1102, LMK1C1103 in the next datasheet revision.
Kind regards, Lane
Hello Vikram,
>Can you please share the voltage swing level of net CLK25MHz_NET1 and the source of it? Is it coming from another 869 phy?
swing level of net CLK25MHz_NET1 : Vh=1.77V , Vl=0.05V
Soure of it : Vh=3.3V , Vl=0V
The output of the clock…
Hi Arief-san,
Thank you for your prompt reply.
I would like to use the low cost clock buffer such as CDCLVC1103. Therefore, please tell me how to use the termination resistor more than 50Ω if possible.
Best regards, Kato
Part Number: CDCM9102 Other Parts Discussed in Thread: CDCLVC1104 , CDCLVC1103 Hello.
Can I input a clock that is not a crystal to CDCM9102? I would like to input the 25MHz output of CDCLVC1104 or CDCLVC1103 to the XIN terminal of the CDCM9102. Is it possible…
Part Number: CDCE913 Other Parts Discussed in Thread: CDCLVC1103 Hi,
I have an application where I need to drive 3 20 bit sigma delta ADC's with a clock. I was originally using a CMOS oscillator with a 45% - 55% duty cycle specification thru a CDCLVC1103…
Part Number: LMX2582 Other Parts Discussed in Thread: CDCLVP1204 , CDCLVC1103 Hi team,
The customer would like to use CDCLVP1204 + LMX2582. The input frequency is 100MHZ. He needs to output 100MHZ, 2GHZ and 4GHZ.
The output frequency 100MHZ is used as the…
Part Number: CDCLVC1310 Other Parts Discussed in Thread: CDCLVC1104 , CDCLVC1103 , LMK00804B , LMK00105 Is there a 3-4 output flavour of CDCLVC1310 also available?
Part Number: CDCLVC1110 Hello support team,
I have a question regarding CDCLVC11xx.
- Can CDCLVC11xx drive a CMOS IC (Vcc = 3.3 V) whose input capacitance is 20 pF with 50 MHz clock signal?
The period of 50 MHz clock signal is 20 ns. So I think the minimum…