Other Parts Discussed in Thread: CDCLVD1208 RE: CDCLVD1208 questions
1) I am not using the differential input 0, should I connect the inputs as follows :
INP0 - 1K pull-up to 2.5V supply rail ?
INN0 - 1K pull-down to ground?
2) The spec mentions…
Part Number: LMK04610 Other Parts Discussed in Thread: CDCLVD1208 Hi,
In Sysref output mode, to you have any recommandation to drive LVDS input with proper common mode ?
Regards,
Hi Ohad,
Refer to 2.5V differential output clocks
www.ti.com/.../products.html
For example, CDCLVD1208
www.ti.com/.../cdclvd1208.pdf
3.3V LVCMOS input could be divided by resistors in 2.5V for CDCLVD1208
Best Regards,
Shawn
Part Number: CDCLVD1216 Other Parts Discussed in Thread: CDCLVD1208 , Hi Ti experts,
We have some doubts about power supply for clock buffer cdclvd1216 and cdclvd1208.
As we search from the datasheet, there are no special requirements for power supply, such…
Hi Suresh,
Please see table on Page 5 of the datasheet: www.ti.com/.../cdclvd1208.pdf
Supply current at Fin = 100 MHz and all outputs loaded = 62mA (Typ) and 84mA (Max). Power dissipated at 2.5V (mW) = 2.5V * 62mA
Regards
Arvind Sridhar
Other Parts Discussed in Thread: CDCE18005 , LMK00306 , CDCLVD1208 , CDCUN1208LP , LMK04828 , LMX2581 , LMK00304 , LMK00101 Hello,
I would use a CDCE18005 as a reference clock mux and fan out buffer, and I would know the total jitter (possibly the max value)…
Other Parts Discussed in Thread: CDCE72010 , CDCLVD1208 Hi,
The ref and VCXO inputs have a hysteresis option, but I don't see any discussion of exactly what the parameters of the hysteresis are. Is there some guidline on when hysteresis should be used…
Hi Jim,
What type of cycle to cycle jitter is needed? From the measurements in the app note, the number could theoretically be close to 170ps (this may be a little pessimistic since the measurments in the app notes are peak to peak jitter). Since jitter…
Other Parts Discussed in Thread: CDCE72010 , CDCLVD1208 I have a system with 8 CDCE72010 clock drivers. I need to set up all the dividers and then have them synchronized over the entire system. I expect I need to use the nReset hardware input to do this…