Looking at the CDCM61002 datasheet it says:
"For proper device operation, the reference input must be stable at the start of VCO calibration. Since inputs from crystals or crystal oscillators can typically take up to 1-2ms to be stable, it is recommended…
Part Number: TMS320C6671 Hello Champs, Customer failed to initialize SRIO when connecting c6671 to FPGA, PORT_OK is always 0. 1. C6678+FPGA SRIO can connected successfully. 2. C6671 SRIO loopback is OK and FPGA SRIO loopback is OK. 3. POR#、RESETFULL#、RESET#…
Part Number: CDCM61001 Other Parts Discussed in Thread: CDCM61002 Hi sir / madam,
I have used CDCM61002 in my project, which is having 2 clock output, but now we need only 1 clock output. So i am planning to replace with CDCM61001. I am using CDCM61002…
Other Parts Discussed in Thread: CDCM9102 , CDCM61002 In developing the new platform product, we consider expanding 1 Ethernet port through the PCIe interface of DRA624. At present, the following technical problems are encountered.
1) about PCIe clock,…
In developing the new platform product, we consider expanding 1 Ethernet port through the PCIe interface of DRA624. At present, the following technical problems are encountered.
1) about PCIe clock, is it necessary to use cdcm9102 or cdcm61002 high precision…
Other Parts Discussed in Thread: CDCM61001 , CDCM61002 I am using both the CDCM61001 and CDCM61002. I am planning on using their LVDS clock outputs and do not require the use of the OSC_OUT (Bypass LVCMOS output) What should I do with this unused pin in…
Other Parts Discussed in Thread: CDCM61002 I use Dm8148 as a pcie RC, C6657 as a pcie EP.Now 8148 cann't scan c6657 at all, lspci show nothing.
Can any one tell me how to fix this.
Use Case
1.Rc and Ep use the same source 100M clock from Cdcm61002. …
Other Parts Discussed in Thread: CDCM61004 , CDCM61001 , CDCM61002 , CDCM6208 Looking for 3 clock generator devices,with input of 25MHZ to generate:
1. 4 outputs of 200M each (like NB3N51034 form ON)
2. 1 output od 200M each (like NB3N3002 from On)
3. 2 output…
I don't see anything similar. The CDCE913 is pin or i2C prgrammable, but only 1/2/4/8 and XTAL MIN is 8MHz.
The CDCM61002 is also pin programmable 1/2/3/4/6/8, but 25MHz XTAL.
As you stated, the IDT ICS525 has a 5MHz XTAL and 7-bits of programmability…
Other Parts Discussed in Thread: CDCM61002 Hello,
The clock generator used in evm816x_Schematics_RevE.pdf (CDCM61002) has LVDS outputs. Can I use HCSL output clock generator and connect it directly to SERDES_CLK pins of C6A8168?
Thank you,
- Robert …