Other Parts Discussed in Thread: MSP430F5438 Hi all, I have a problem connecting USB to UART with IAR Embedded Workbench. I am using the device below which includes CP2102 USB-UART serial converter.
IAR cannot recognize the converter and I cannot…
I'm trying to use the BSL with the MSP430F5438A Rev F, which should not have the timing issue according to the errata sheet. I'm using it with the CP2102 USB to serial converter with the same settings as listed previously in this post:
CP2102 MSP430F5438A…
Part Number: TUSB8020B-Q1 Other Parts Discussed in Thread: HD3SS3212 Tool/software: Hi everyone,
I designed a USB 3.0 hub using TI TUSB8020BPHP with Type-C upstream and downstream. Downstream Port 1 (to a CP2102 USB 2.0 device) works fine, but Downstream…
Hi,
1. Yes this is a custom board.
The waveform attached for SOP PIn and NRST pin in SOP2 mode.
2. USB to UART Converter :
USB-TTL UART Module - CP2102
3. We probe the XTALP, XYALN, VBGAP and NRST in SOP2 mode. The waveform is attached…
Hi Sivaprasad,
R16(and R15) on the pcb has been removed,
Since there are no xds110 and l1432 connections on our board, I directly connected RS232_TX(E10) and RS232_RX(F11) to the computer via cp2102.
I'm not sure whether this hardware connection…
Hi Vaibhav,
I am already refered datasheet and UART3,4 and 6 enable and check data is not coming.UART5 only working CP2102 module UART3,4 and 6 not working CP2102.
Best Regards,
VJPANDI
Hi Vaibhav,
Yes. I telling UART0 connected GPIO pins A5-Tx pin is connected CP2102 Rx pin,B5 Rx pin is connected CP2102 Tx. I attached GPIO pin configuration sysconfig file attached.
How to fix problem.
Thanks Regards,
Veerapandiyan V
Hello,
Thank you for your question. The UART protocol will require the connections: MCU TX to CP2102 RX and the CP2102 TX to the MCU RX. Based on the pin configurations you've listed it sounds like your are using the ISO6721B device with the CP2102…
hi , first thanks for reply.
i also have the doubt for TX and Rx connection of CP2102 to Tx(24) and Rx(25) pin MCU respectively. But when i swapped them it gives Error msg of BSl is locked for Tx_Bsl_Version and Rx_DATA_Block command.
Connection are…
Part Number: ISOW7741DFMEVM Other Parts Discussed in Thread: ISOW7741 , ISOW7721 Hello Team,
I'm evaluating ISOW7741DFMEVM for isolating UART Signals.
My Setup is as follows
CP2102 (USB/UART Converter) TX is connected to INA of the EVM
MCU RX…