Part Number: CSD16415Q5 Dear Team,
Please help me to confirm the lower limit of the Vds specification of CSD16415Q5, whether there is no lower limit requirement or the specification is incomplete, Thanks!
Many Thanks,
Jimmy
Part Number: CSD16415Q5
Hi team,
If Vgs beyond -12V~16V, how long can CSD16415Q5 persist to work?
My customer wonders the device persistence time if Vgs beyond normal range. Please kindly provide the data, thank you!
Best Regards,
Miranda
Hi team,
Thank you for your response. Separately, we are also considering alternative parts.
Can the following parts be used? I do not think there is any problem because of good SOA characteristics. Also, could you please let me know the precautions to be…
Other Parts Discussed in Thread: CSD18533Q5A , LM25118 , CSD16415Q5 Hi, we are a couple of students designing a power for our ECU project.
We've made a design in webench using the LM25118 Buck/Boost controller, which implements both the CSD18533Q5A N-ch…
Other Parts Discussed in Thread: CSD16415Q5
Super quick question…
Do we have any plans to release a simulation model in switcher pro or WebBench for the CSD16415Q5?
Please provide scheduling if we don't....
Thanks
Hi Nikesh,
The device on Mouser is a different part number, CSD16415Q5, with higher on resistance: 1.15mΩ max vs. 0.59mΩ max at VGS = 10V. The CSD16415Q5 is in a different package but should work with the Q5B PCB footprint with no changes. I'm assuming…
Wells,
Thank you for your interest in our MOSFETs.
As the CSD16401Q5 data is not on the TI website I am working to get this corrected ASAP.
if you can not wait for an answer then I suggest you use the CSD16415Q5 which is on the web here: https://www…