Part Number: CSD19536KTT
Hello,
I would like to ask you about the SOA of CSD19536KTT. The attached figure shows the waveform when the FET turns on. Is the behavior shown in this waveform acceptable for SOA? Also, please provide the temperature derating…
Part Number: CSD19536KTT My question is due to our unusual Gate threshold voltage requirement.
The requirement is the following: Vgs <3.65V at Vds=10V, ID=200mA. @TA=25c
The CSD19536KTT device that was tested, passed the test with a Vgs of 3.35V.
…
Part Number: DRV8308 Other Parts Discussed in Thread: CSD19536 , CSD18511KTT , CSD19536KCS , CSD19536KTT Hello,
I use an DRV8308 fo drive an BLDC with 18 Volt and approx 100 Ampere. WIth an IRFS7430 the MOSFET was so warm an a low duty of the PWM, taht the…
Part Number: CSD19536KTT Hi,
I want to design an RCD snubber circuit for my inverter board using CSD19536KTT , I'm unable to select the diode properly, Requesting your support for the design considerations and equations for selecting diode for RCD snubber…
Part Number: CSD19536KTT Other Parts Discussed in Thread: TIDA-00364
We have designed 3 phase full bridge MOSFET based inverter circuit and its Layout for
motor controller application
The Nominal operating voltage is 48 V , Maximum operating DC current is 200A , and pea…
Part Number: CSD19536KTT Other Parts Discussed in Thread: CSD17307Q5A , CSD17304Q3 Hi everyone,
Would you please suggest some mosfet part numbers for my application please ?
Voltage: 24V
Current: 10 Ampers
Trigger will be 3.3V, PWM.
Thanks!
Part Number: BQ76940EVM Hello,
My application requires a continuous discharge current of 30A, which can be easily done by CSD19536KTT
I also noticed that the same FET is being used in TIDA 00792 .
Both have nearly the same Vgth and Rds of CSD19536KTT is comparatively…
Part Number: DRV8353 Other Parts Discussed in Thread: CSD19536KTT , Hello
I have used 12 NMOS CSD19536KTT for 3 phase bldc motor control. DRV8353 is used as predriver and 1mE as current sense resistor for individual 3 phases.
But unfortunately DC current…
Part Number: DRV3256-Q1 Other Parts Discussed in Thread: CSD19536KTT , Hello,
Trying to understand IDRIVE and how to reduce the rise time. The min setting of the pullup current is 1.5A and I am using the CSD19536KTT with a 17nC Qgd charge, so the min rise…