Other Parts Discussed in Thread: CSD88537ND , CSD88539ND , CSD75208W1015 , CSD75207W15 Hello:
Please recommend a general MOSFET (dual MOS) with good relative delivery date and high cost performance.
Demand parameters: package SO-8、RDS (on) = about 100m Ω…
Hi Zhengquan,
Thanks for the inquiry. We have two dual, common-source PFET devices: CSD75208W1015 & CSD75207W15. Please note, our PFET devices only got to -20V max BVDSS. There are many options for dual NFET devices which can be found here: .
Part Number: PGA460-Q1 Other Parts Discussed in Thread: CSD75208W1015 Hi
May i have your suggestion for the Q-grade dual P channel Mosfet for Direct drive ?
Currently EVM are using FDC6506P but not Q-Grade.
Thanks!
Nico,
Looking at the schematic of the CSD75208W1015 on the front page (image below) you can see that the body diode cathodes are connected to the source. If you have a no connect to the sources and simply tie the gates together to allow current to flow…
Dear Brett Barr-san
Thank you for the reply.
Sorry, please let me also know the following by addition.
-----------------------
CSD75207W15 datasheet is written to "Drain1 to Drain2 Voltage" by figure-2.
In contrast,CSD75208W1015 datasheet is…
Michael,
The forward voltage drop across the MOSFET is characterized in Figure 9 of the datasheet. How much current are you pushing through the device?
We actually have some dual common source FET, the CSD75208W1015 chip scale part, but it is not capable…