Part Number: BQ2973 Other Parts Discussed in Thread: CSD85301Q2 Hello Expert,
Our customer have a plan to use BQ29728 or BQ29737.
As you know, there is lead time issue recently.
So our customer want to use CSD85301Q2 which is stock in TI.COM.
Below is their…
Part Number: DRV8305-Q1 Other Parts Discussed in Thread: CSD18540Q5B , CSD85301Q2 , DRV8305 hello
The FET on DRV8305-Q1 EVB is CSD18540Q5B (Rds=3.3mOhm), I want to use automotive FET, I found CSD85301Q2(Rds=23m Ohm) part number.
The current of my motor is…
Hi Nikos,
This element is part of the symbol for the CSD85301Q2 FET. You can see in the datasheet for this device that there are two diodes back to back between the gate and source.
Best regards,
Matt
na na78 said: 1. In this power map, TPS544C25 is used to supply 0.72V which is different voltage level with VCCBRAM. The purpose of TPS544C25 implemented is just to supplying different voltage with BUCK2, isn't it? Yes and no. TPS544C25 can be used…
Other Parts Discussed in Thread: CSD86311W1723 , CSD85302L , CSD85301Q2 Hi,
We are planning to use n-channel e mosfet between battery and rest of the circuit.
We need the mosfet to turn off when gate voltage is low and turn on when gate voltage is high. …
Part Number: TPS650864 Other Parts Discussed in Thread: CSD85301Q2 , Hello guys,
One of our customers is considering to use PMIC, TPS65086470 for Artix-7.
Then they want to know what the following pins setting should be set to because they don't need BUCK6…
Other Parts Discussed in Thread: TPS65086 , MSP430G2121 , TPS65023 , CSD87353Q5D , CSD85301Q2 I am using two Arria-10 FPGAs in a new design and am looking for advice on a discrete design such as produced by Webench, vs using a PMIC such as the TPS65086x family…