Part Number: LM5100A Other Parts Discussed in Thread: CSD88539ND , , LM5101A When using the LM5100AM Gate Driver according to the typical application circuit shown in the data sheet, LO and HO signals when probed do not show the expected outputs. I believe…
Hello Darren,
Thanks for the inquiry. The CSD88539ND is a p2p 60V dual NFET with lower on resistance at VGS = 10V (28mΩ vs. 35mΩ max). Please note, the CSD88539ND requires VGS >= 6V whereas the competition is rated down to VGS = 4.5V. The TI device is…
Part Number: DRV8300 Other Parts Discussed in Thread: CSD88537ND , CSD88539ND , CSD88599Q5DC Hi team,
Here's an issue from the customer may need your help:
The customer is looking for a dual integrated NMOS used with DRV8300, the requirements are as…
Part Number: CSD88537ND Other Parts Discussed in Thread: CSD88539ND , CSD17577Q5A I know this is a long shot, but I am supporing a request for a replacement to HAT2195R.
Datasheet
This device has an SO-8 package, but the only "same package" I can find …
Other Parts Discussed in Thread: CSD88537ND , CSD88539ND , CSD75208W1015 , CSD75207W15 Hello:
Please recommend a general MOSFET (dual MOS) with good relative delivery date and high cost performance.
Demand parameters: package SO-8、RDS (on) = about 100m Ω…
Other Parts Discussed in Thread: CSD18541F5 , CSD18543Q3A , CSD19538Q3A , CSD88539ND , CSD19538Q2 Hi,
I have a query regarding selection for PMOS, NMOS, or complementary mosfet.
Requirement is to find mosfets for the switching of 500KHz frequency, so what…
Hi Jim,
Thanks for your interest in TI FETs. The CSD88539ND is a dual 60V NFET in SO8 package. The CSD18541F5 is a single NFET in F5 FemtoFET package with about double the on resistance per FET. You may be able to parallel 2 of these to get approximately…
Hi Jimmy,
Thanks for the inquiry. Do the FETs need to be automotive qualified? If so, then TI does not have any auto-qualified FETs and we do not plan to qual any of our devices to automotive standards. I am including a link below for TI FET selection…
Hello Yamaguchi san,
Thanks for promoting TI FETs at your customer. Our closest cross to the Toshiba device is the CSD87502Q2. This is a 30V, dual NFET in 2x2mm SON package. TI doesn't make more than 2 FETs in a single package and we do not have any dual…