Hi Scott,
The only dual part we have with symmetric FETs that may work for your application is the CSD87333Q3D. It's in 3.3 x 3.3mm QFN style package. Please note, the VGS is rated at 10V abs max for the FETs with a recommended max operating of 8V. Therefore…
Part Number: DRV8323 Other Parts Discussed in Thread: CSD88584Q5DC Hello,Everyone,
I have a problem that DRV8323H is hot. I use a combination of TMS32F28027F and DRV8323H, and CSD88584Q5DC 40-v half-bridge.
Under the condition of no load, each time the…
Part Number: DRV8323R Other Parts Discussed in Thread: CSD88584Q5DC , CSD , DRV8306EVM , DRV8323 5 questions if I may;
1. Is there anything that would stop us using DRV** (for example DRV8232) + CSD** (for example CSD88584Q5DC) in high-end sinusoidal inverter…
Part Number: DRV8323R Other Parts Discussed in Thread: CSD88584Q5DC , DRV8323 , CSD88599Q5DC My motor driver is implemented using the DRV8323RX+CSD88584Q5DC
In the application, a mismatch between the gate drive signal and the PWM signal is encountered, causing…