Part Number: CSD95492QVM Hi,
While going through the datasheet, i didnt find the criteria and resistor selection method, please help me to find the way how to select the resistor value for it.
Thanks
Vikas
Part Number: CSD95492QVM Dear Team,
May I know the power consumption for the VDD pin.
The customer is wondering about the suitable LDO for all of the power stage.
Can I said one CSD95492QVM's consumption is 5V*12mA?
BR
Kevin
Part Number: CSD95492QVM NexFET has unique clamping diode to reduce switch node voltage.
What is the avalanche voltage for the clamping diode?
Is there power dissipation limit for the clamping diode?
Part Number: CSD95492QVM Other Parts Discussed in Thread: CSD95490Q5MC , Hi,
Similar to the question in: https://e2e.ti.com/support/power-management/f/196/t/663588
1. I'm looking for the Rlset equation for CSD95492QVM, does it match the equation in the…
Part Number: TPS53622 Other Parts Discussed in Thread: CSD95492QVM Hi,
I have TPS53622 setting questions as follows, thanks.
1. How to set the TPS53622 SVID Address? Is there a relevant table for reference?
2. How to configure if TPS53622 B SENSE is not…
Part Number: TPS53647EVM-710 Other Parts Discussed in Thread: CSD95492QVM , TPS53647 Hi,
We need some technical help on a PoE+ related Buck converter issue. The max energy for PoE+ is 25.5W. We have a communication system that is duty cycled between transmit…
Other Parts Discussed in Thread: CSD95495QVM , CSD95492QVM The CPU solution is denverton, and the vid version is vr13,
The requirements are as follows: the maximum power consumption is 30W, and four power supply channels are required.
Pvcc 1.05v 30A svid_…