My Vdd is 5V, and it is used all around the analog portion of the device, and in some devices (I also have DAC128S085 where I use it as both the Va and the Vref), so I would have to implement a separate 5.5V (the thread you showed says 5.2V is also OK…
I tried changing the install path to `/opt/ti/c2000` but it is still not found:
root@53c4521b41b5:/home/app# ./resources/C2000Ware_5_00_00_00_setup.run --mode unattended
root@53c4521b41b5:/home/app# ls /opt/ti/
'Code Composer Studio 12.6.0.desktop'…
Part Number: TMS320F2800137 Other Parts Discussed in Thread: SYSCONFIG , C2000WARE , TIDM-02010 , SFRA , DAC128S085 Dear Sir,
Please find the attched copy of Full code & check Error..
ODU_TI_Project_ADC_03012024.zip
Please check & resolved.
Part Number: DAC128S085 Hello,
I am wndeing if someone could please tell me if DAC128S085CIMT/NOPB and DAC128S085CIMTX are interchangeable?
Or what are the meanings of the additional letters on the end of the part numbers,
NOPB
X
Thanks!
Colm.
Part Number: DAC128S085 Other Parts Discussed in Thread: ADS7044 , Hi all.
In my project, I'm thinking to use DAC128S085 and ADS7044. I'd like to connect the two devices with the microprocessor by the same SPI line (the microprocessor is the MASTER…
Part Number: DAC128S085 Other Parts Discussed in Thread: CC2500 I have problem programming the DAC128S085. I attached my SPI timing. I am broadcasting a 4V reference. But no output voltages. Please help
Ryan Ma said: Are you using the motorcontrol sdk?
i am using this sdk:C:\ti\c2000\C2000Ware_MotorControl_SDK_5_00_00_00\c2000ware
Ryan Ma said: Can you remove these files from the project? sw_interrupt_prioritization_logic.h, sw_prioritized_isr_levels.h…
Part Number: DAC128S085 IF DAC DOUT signal is tri-state, can this parts be used on SPI bus with other SPI devices or does it need try-stated buffer on DOUT signal
Thank you,
I don't see the DOUT voltage level (VOH) called out in the datasheet. There's an output voltage section, but I believe this is just for analog voltages. If VREF = 2.5V and VA = 5V, can we expect the DOUT pin high level to be 5V? We are using an SPI master…
Other Parts Discussed in Thread: DAC128S085
Hi there,
I'm having a little trouble with the DAC128S085 that maybe someone else has seen before. It seems that the DAC is driving some voltage into the serial pins for the first couple of clock cycles. I…