Part Number: DAC3151 Tool/software: Hi Team,
Do you have a method for testing settling time? The capacitive load of DAC3151 is very low, just 5pF. The settling time is about 11ns. It is difficulty to test the settling time using a MSO oscilloscope.…
Part Number: DAC3100
Hello,
I have a question and would appreciate your support.
I am using the DAC3100 with the following configuration: P0 / R27 = 0x3C (I2S, 32-bit, BCLK = output, WCLK = output). When changing the sampling rate, a large amount…
Part Number: DAC3151 Other Parts Discussed in Thread: DAC3174 , Tool/software: Hi all,
I could not find the DAC3151EVM software.
I am looking for the DAC3151 software "DAC3174 Software" listed in the 2.1 Installation Instructions below.
DAC31x1EVM…
Part Number: DAC3151 Hello Team,
to produce a periodic output signal it seems from first evaluation on the hardware mounting the DAC3151 that a SYNC is required by any write.
In the datasheet does not seem that this is really needed. Can you confirm…
Part Number: DAC3151 Other Parts Discussed in Thread: CDCE62005 Hi
For DAC3151, please help with below questions. Thanks!
1.What is the relationship of DATA CLK and DAC CLK? If data rate is 400MHz, then DATA CLK and DAC CLK are both 400MHz?
2.Is…
Part Number: ADS4146 Other Parts Discussed in Thread: DAC3171 Hello all ,
I want to connect an 14 bit adc (stated in the headline)with parallel lvds output to a 14 bit dac (stated in the headline) that works with serial input .
is it possible ? if…
Hello Team,
I'm trying to better understand the timing requirements shown on paragraph 6.8 related to the LVDS INPUT TIMING of the datasheet.
In particular Figure 1 shows that the bit is made of ts(DATA) and th(DATA).
From the table, taking the…
Hi Richard,
I want to set DAC3151 in FIFO bypass mode.
Can we by-pass FIFO in DAC3151 for normal operation (Data and DAC clk matching will be taken care)? If we disable the FIFO then do we need to provide sync signal to DAC ?
We are using below…
Other Parts Discussed in Thread: DAC3151 For many DAC chip, using the default mode after power can work. But why can not I use the default mode with DAC3151.
Other Parts Discussed in Thread: DAC3151 Hi
We are planing to use DAC3151, our application requires to vary the sampling frequency from 5MSPS to 160MSPS. can we use DAC3151 at lower sampling
frequency also?. The datasheet does not mention a minimal…