Part Number: DAC3283 Other Parts Discussed in Thread: ADS62P49 I am working on DAC3283 eval board SPI interface with zcu106 FPGA evaluation board using FMC connector. For that we have used FMC DAC adapter(from TI). But when we referred to the schematics…
Part Number: DAC3283 Hi,
I have followed the section 10.1 Power Sequence of the datasheet to initialize the DAC device. I checked for any errors or alarm registers triggered and there were none.
Next, I ran an I/O pattern check by enabling bit 2 of Config1…
Part Number: DAC3283 Hi all,
I'm working with DAC3283 device on a new project. The device is assembled in a PCB with an FPGA and DSP devices.
I'm trying to configure the DAC with SPI interface but there are some issue.
First of all I have setted…
Part Number: DAC3283
Hi,
I saw a forum post earlier mentioning about using this DAC to support two real data inputs. It mentioned that I should not use the complex mixer or QMC functions.
I am wondering which registers I need to setup for only "real"…
Part Number: DAC3283 HI!
I am planning to use DAC3283 for the below application and i have the below query,
Application:
DAC CLK: 4000MHz
Output Freq: 75 MHz
Query:
1)I have only CML clock outputs in my system with VOD=420mVpp (typ). Is there a way to…
Part Number: DAC3283 We are planning to use IC DAC3283IRGZT in our board design. dr-ve-10-mo_datasheet.pdf
We want to connect DAC output to RF amplifier having input impedance of 50 ohm.
We have 2 RF amplifier, so we will use IOUTA1 for first RF amplifier…
Hi Kang Hsia,
Thanks for your reply.
Please reconfirm whether the device to device variation of DAC3283 (100ps typical), will it be deterministic/Constant per device or will it vary from power on to power on?
if it is not varying per chip then Is it possible…
Part Number: DAC3283
HI TI Team,
In the thread " ">e2e.ti.com/.../dac3283-phase-noise-detail-of-the-part-reg" , I enquired about the close in phase noise data (from 10Hz of fundamental) of DAC.
NSD plots of the part was shared as reference…
Part Number: DAC3283 Other Parts Discussed in Thread: CDCE62005 , Hello,
I am using custom board which has an interfaces of DAC (DAC3283 ) and Clock Synthesizer (CDCE62005).
For DAC it is 16 bit with 800MSPS DAC output and 8-Bit Input LVDS Data Bus .
I…
Part Number: DAC3283 Hi,
We are planning to use the DAC3283 in our project design, Kindly share the phase noise of the DAC's output. Refer the below details.
Clock input : 800MHz
Output frequency : 300MHz
Note : PLL(if provided internally) to be…