Part Number: DAC34SH84 Hi all,
My customer would like to know the performance of near spurious noise of DAC34SH84. Their test results of 184.32MHz +/-62.5kHz was about -62dBc/100kHz. DACCLK was 732.78MHz and its phase noise at 62.5kHz is -126dBc/Hz. And…
Part Number: DAC34SH84EVM Hello,
I am trying to make automated code for the DAC34SH84EVM similar to the high speed data converter pro automation DLL, something that is very user friendly. I have been using the labview code from a post I found in the E2E…
Part Number: DAC34SH84EVM Hej,
Is there anybody having the same problem with physical connection of the DAC34SH84? The yellow locking part doesn't fit to both holes of the adapter.
Thank you for your help.
lONG
Part Number: DAC34SH84EVM Hej all,
I am using DAC34SH84EVM rev D (which I guess it is reference D) and FMC-DAC adapter rev D. I did cut off the tab to make them being able to connect.
Now I have another issue that make me confused
1. At DAC34H8x EVM Interface…
Other Parts Discussed in Thread: DAC34SH84 , FMC-DAC-ADAPTER Hello,
I recently purchased a DAC34SH84 EVM board and a FMC-DAC-Adapter to connect the EVM to a FMC connector on a Xilinx board. The problem is that the DAC34SH84 has a 180 pin HSMC connector,…
Other Parts Discussed in Thread: DAC34SH84 , DAC3484 Hello,
I am using DAC34SH84 EVM Software version 3.8 to configure DAC34SH84 evm board. Problem is when ever I am changing any options in GUI by computer mouse is it coming back to some default value.…
Hello everybody,
I was following the steps in DAC348x EVM manual: http://www.ti.com/lit/ug/slau432/slau432.pdf testing with TSM1400. The DAC I am using is DAC34SH84 EVM and at 3.4 DAC348x Example Setup Procedure, I provided clock input of 1474.56MHz with…
Part Number: DAC3482EVM Hello team,
I am using DAC3482EVM with TSW1400EVM.
On the p.9 of the DAC348xEVM user's guide, it says,
Y3: FPGA Clock 1. This clock is an ac coupled LVDS. The clock rate for this should be
– F DAC /interpolation/2 for …
Other Parts Discussed in Thread: DAC34SH84 , TRF3705 Dear,
1. Maximum analog of DAC34SH84 is input data rate(Fdata)*0.8. correct?
2. if correct, with interleaving, maximum Fs 1.5GSPS*0.8=1.2GHz max analog output?
3. Then how many dB is filtering loss? if…
Other Parts Discussed in Thread: DAC34SH84 Good Morning.
In our design we are using the DAC34SH84 without interpolation at 625 MSPS. As far as I can tell the device requires a 625 MHz reference on both DACCLK and DATACLK. Is this correct or does the reference…