Part Number: DAC38RF80 Hi TI, I am using dac38rf80 in 88210(2 TX ) mode with x24 interpolation on our custom PCB. 1. sync signal is not toggling . it stays 0 after reseting dac jesd core. 2. after reading alarms a) I am getting 0x64 to 0x6b is 0x0 b) 0x5…
Part Number: DAC38RF80
Hello,
In a previous post ( https://e2e.ti.com/support/rf-microwave/f/220/t/903004 ) I asked if it was possible to set up the DAC38RF80 to be single DAC mode, so all 8 lanes are for a single DUC (LMFS = 8212), and have that output…
Part Number: DAC38RF80 Hello,
The DAC38RF80 allows three ways (section 8.3.8 of the data sheet) to set up the link to the DACs through the JESD interface: Dual DAC dual link, Dual DAC single link, and Single DAC single link.
For Dual DAC single link,…
Part Number: DAC38RF80
Hi TI,
We are using DAC38RF80 in our design which is a single ended output DAC.
I have a query regarding the the resistors used on output of DAC38RF80 Eval Board.
What is the purpose of these resistors? Do they function as attenuator…
Part Number: DAC38RF80 Other Parts Discussed in Thread: LMX2582 , Hi,
Can I use LMX2582 output as a reference clock input for DAC38RF80 DACCLK pins?
Thanks,
Lalit
Part Number: DAC38RF80 Hello,
I'm trying to understand how to use the SYREF capture circuit statistics described in the DAC38RF80 datasheet. In our design, we use an LMK04280 to drive the device clock and sysref for the DAC38RF80.
What are the minimum…
Part Number: DAC38RF80 Hi TI,
We are using DAC38RF80 in our project. We have completed the design.
Now we want to do the simulation of the JESD interface between DAC and FPGA.
IBIS model of DAC38RF80 is available on DAC38RF80's TI page.
But we require…
Part Number: DAC38RF80 hi,all
I have some questions about DAC's link configuration:
1.This DAC support dual link mode, it means one channel is a link,another channel is another link. Does it need to the LMFS parameter is the same for each link? …