Part Number: DAC38RF89 Other Parts Discussed in Thread: DAC38J84 Hi guys,
My customer is using the DAC38rf89 in a design and has the following questions:
We are having some issues with the DAC38RF89 JESD interface. We have been able to pass the PRBS…
Part Number: DAC38RF89 The description in the datasheet sound like the device indicates too much or too little but need to isolate which is the problem. On some lanes see that both EQOVER and EQUNDER are asserted (other lane are fine). We have the DAC…
Part Number: DAC38RF89 Hello,
I'm trying to verify the frequency change after writing the 3 (16 bit) NCO registers. I can write them and then check the SIF SYNC box on the gui and the NCO changes frequency. I wrote to registers 0x11E, 0X11F, and 0x120…
Part Number: DAC38RF89 DEAR:
Thank you first for your answer,but I want to ask another question .
I am using the DAC38RF89 ,and LMFS = 8118 ,but I changed the serdes rate = 6G,the DAC_CLK = 4.8G derived from the DAC PLL ,
the dac_clk_in from the…
Part Number: DAC38RF89 DEAR:
I am using the DAC38RF89 ,and LMFS = 8118 ,the serdes rate = 3G,the DAC_CLK = 2.4G derived from the dac_clk pin directly,but I cannot get the ANALOG OUTPUT, I just get the constant Output by 0x12F 0001.
can you give me…
Part Number: DAC38RF89 Dear:
I met a problem ,when I using the DAC38RF89.I choose the register of 0x12F_0001 ,get the constant output of a sine wave,but when I change the register to 0X12F_0000,there is nothing out. I got the 204b communication was…
Part Number: DAC38RF89 Dear colleagues, my customer is interested in phase noise of DAC38RF89 - dBc/Hz
Where is it possible to get the data?
Thanks,
Vladimir.
Part Number: DAC38RF89 Other Parts Discussed in Thread: , DAC38RF82 I have a DAC38RF89EVM board connected to a KCU105 board via the HPC FMC connector. I am following this guide on running an example reference implementation.
I have programmed the FPGA…
Part Number: DAC38RF89 Tool/software: Starterware hello
I want to use dac38rf89evb with tsw14j57 ,
but there isn't the firmware in The hsdc pro ,
so I want to have the firmware and the dac" .int "file in hsdc pro.
I need help
thankyou
Part Number: DAC38RF89 Hello team,
Hope you are well. Can you provide some feedback on below questions:
Is there an IBIS AMI model for the highspeed pins on this part? This is a high speed DAC with a high speed clock and SYSREF along with JESD lanes. …