Part Number: DAC38RF89EVM DAC38RF89 GUI questions.pdf I am looking for a user's guide for the DAC38RF8x GUI that shows what the fields are to fill in and where one gets the information from the datasheet to load it in. Please see the attached PDF with…
Part Number: DAC38RF86 Other Parts Discussed in Thread: DAC38RF89 Hi,
I'd like to generate four complex modulated carriers:
Two at 875 MHz (each 250 MHz Bandwidth)
Two at 1125 MHz (each 250 MHz bandwidth)
Is this feasible? If so, I need to know…
Dr. Reeves,
The DAC38RF83 has a max input data rate of 1.25Gsps, so you will not be able to send data at 1500Msps. You can use this data rate if you switch to either a DAC38RF82 or DAC38RF89. This is why you see the numbers you do in table 9. I will look…
Part Number: DAC37J82 Other Parts Discussed in Thread: DAC38J84 , DAC38RF89 , DAC38RF84 I am evaluating the DAC37J82 for direct RF synthesis at 1 - 2.6GHz testing various nyquist zones. The spurious response is good, but when I generate two tones the IMD…
Hi Jonathan,
This is an error in the GUI. It should be possible to select 16x interpolation for the mode you are trying to use.
Can you replace the following file with the one attached: modes_n_clock_programming.tx t
The file can be found in C:\Program…