Part Number: DAC5675A-SP Other Parts Discussed in Thread: DAC5675 , DAC5675A , CDCLVP111-EP , SN65LVDT101 We are using the DAC5675 on a space project (LEO missions) and we are thinking about driving the clock_p and clock_n with LVDS signals generated from…
Part Number: DAC5675A-SP Hi team
Customer wants to understand the time for the device to get back to normal mode from sleep mode. I mean, how long does they need to wait to use the deivce as normal mode afther that the sleep pin level become low from…
Part Number: DAC5675A-SP Hi Team,
Good day! Could you help to clarify the rated supply voltage of DAC5675AHFG. As our customer noticed that both absolute maximum ratings and Recommended Operating Conditions table show the same value 3.6V for supply voltage…
Part Number: DAC5675A-SP Other Parts Discussed in Thread: DAC5675A I'd like to clarify the amplitude requirement for the clock input of the DAC5675A-SP. data sheet gives the following spec:
Is this equivalent to the following LVPECL type differential…
Part Number: AFE11612-SEP Other Parts Discussed in Thread: ADC128S102-SEP , DAC5675A-SP , While analyzing the IC datasheet and comparing it with the other ADCs and DACs available in the TI product selector list, some queries were raised.
Kindly provide a…
Other Parts Discussed in Thread: DAC5675A Hello;
I need a schematic detailing connections to 5962-0720402VXC: External Clock
Power Supplies.
Passive compoments
Thank you
The output voltage of the DAC must remain between 2.3V and 3.6V for an AVDD of 3.3V. The device will not operate correctly if this is not respected as the internal circuitry needs this headroom to function properly.
Thanks
Christian
Hi,
The maximum specs are based on statistical analysis of empirical data measured with the device in an operational mode with maximum Iout(FS), a clock speed of 400MHz, and an Fout of 70MHz. So while it is true the digital power dissipation will never…
Part Number: DAC5675A-SP We use the DAC5675A-SP to synthesize the transmit signal of one of our spaceborn systems. We plan to use the EXTIO voltage for the adjustment of the output power level. Hower the dynamic range, which corresponds to the recommended…
Part Number: DAC5652-EP Other Parts Discussed in Thread: DAC5675A-SP Hi,
I would be interested to use the DAC5652-EP converter for a space radar, because it is dual-channel, its architecture is quite simple, it has a satisfying resolution and it looks…