Dear Neeraj,
Sorry i couldn't follow it due to some reasons.
I made the setup as per the value suggested by you of 0x50EF.Following are the DAC settings--
DATACLK = 120MHz
DACCLK = 480MHz
Interpolation = 4
NCO = 10MHz
QMC =OFF
PLL = Off
SER_DAC_DATA…
Other Parts Discussed in Thread: DAC5688 , DAC5687 , DAC5686 Dear all,
the pll clock mode of dac is used. This SE-clock from the clock distributor is inputted to the pll of DAC5688. The output of the pll will be used as the internal clock of DAC. However…
Other Parts Discussed in Thread: DAC5688 Hi, I am using a DAC5688 with a Pentek 5973 VPX carrier card, and having some problems with -60dBc spurs +/- 40MHz from my test CW signal. I am feeding a CW signal using interleaved data mode to the DAC5688 at 200MSps…
Part Number: DAC5688EVM Other Parts Discussed in Thread: DAC5688 , CDCM7005 I have installed the S/W from both the CD and the web and the DAC5688 driver shows up as "Other devices" DAC5688 driver unknown. I am using this attached to a TSW1400EVM…
Other Parts Discussed in Thread: DAC5688 Hello,
1). I use DAC5688 in External Clock Mode. the PLLEnable=disabled. PLLSleep = sleep.
Do I still need to concern about the PLL_range and PLL_gain, PLL_m, PLL_n settings?
2). My Input clock is 250MHz. If using…
Other Parts Discussed in Thread: DAC5688 When I install the software for the DAC5688 EVM, the USB drivers do not get installed. There is a DAC5688 drivers directory that gets installed, but Windows Device Manager shows the device as having no driver. Even…
Other Parts Discussed in Thread: DAC5688 , CDCM7005 , DAC3282 , DAC3283 Hi,
What High Speed Data Capture and Pattern Generation Platform should be used with the DAC5688 and DAC5589?
The Customer has a TSW1400EVM, but it doesn’t look like the TSW1400EVM…
Other Parts Discussed in Thread: DAC5688 I have questions about the DAC5688.
I using the DAC5688 chip as a DUC(Digital Up Converter).
DAC5688 input data are I, Q values. (IQ sampling)
And I using FMIX(Full Mixer) and NCO.
Question1) When the DAC input clock…
Other Parts Discussed in Thread: DAC5688 Hi,
I would like to confirm the behavior of DAC5688/9 under the "dual bus modes".
In this mode, we can use DAC5688/9 as complete individual 2 ch DACs, correct?
Sorry for my basic question.
Best Regards…
One simple question: Are re-quantisers implemented after each FIR Filter?
We currently estimate that the outputs of the FIR Filter is re-quantisied back to 16bit. Could you please confirm?
Erik