Other Parts Discussed in Thread: DAC5689 Hi all
There is a question by setup of DAC5689.
Table 5. Register name: CONFIG3 Address: 0x03, Default 0x00 Bit 7 Bit 6 Bit 5 Bit 4 Bit 3 Bit 2 Bit 1 Bit 0 diffclk_dly(1:0) clko_dly(1:0) Reserved 0 0 0 0 0 …
Hello
I would like to know is the below configuration possible or Not.
The DAC has 2 path, I want to put different frequency respectively channel1 and channel2.
I t means that the ouput frequency of DAC1 is 25MHZ and the other one's frequency is 75MHZ.…
Other Parts Discussed in Thread: DAC5688 , DAC5689 , DAC3482 Hi~
Our customer will use DAC5688 or DAC5689.
In DAC5688/DAC5689 Part,
Can we output On/Off for IOUTA and IOUTB Individually ?
Please recommend related register parameter and value...
If can't adjusted…
Other Parts Discussed in Thread: DAC5689 , LMK04033 I have a customer who is using the DAC5689 on an existing production board. He configures the device to be in half rate bus mode. He used both data buses and hios issue is when CLK1 is at 200MHz, CLK2…
Other Parts Discussed in Thread: DAC5689 Dear sir /madam,
I have a problem when I use TI DAC5689: my system clock is 100MHZ, (the frequency of the signal which I sent to DAC5689 is 1MHZ) ,how I set the CLK1 and CLK2 of DAC5689 ? I use differential clock…
Other Parts Discussed in Thread: DAC5689 Hi
First of all sorry for my Engish , i'm not the native speaker, but here is my problem:
I've bought DAC 5689 EVM board for broadband signal generation (for example LFM with band width about 40 -60 Mhz)…
Other Parts Discussed in Thread: DAC5688EVM , DAC5688 , DAC5689 DAC5688EVM and TSW1400EVM tend to be used and it is going to output the following frequency.
Is it right at an attached register setup? If a mistake occurs, please let me know.
7522.DAC5688_data…
Other Parts Discussed in Thread: DAC5687 , DAC5688 , DAC5689 Hi,
I'm in the process of selecting Transmit DACs for our new SDR project.
The power consumption details of TI DACs are not mentioned in detail in
the datasheet. Only the worst case specification…