Part Number: DAC60096 Excuse me, our lab need multi DACs board for silicon photonics optical switchs array ,about 256, and we consider achieving it with 3 DAC60096.
However, the official website only offer a gui exe. As for our application , we need operate…
Part Number: DAC60096 Hi,
What is the maximum slew rate can be achieved for properly buffered (with fast precision op amps) DAC60096 outputs?
Thanks,
Nikolai
Part Number: DAC60096 Hi,
Question about DAC60096 96-Channel part.
What is the amount of time all the 96 Channels are updated ?
I`m not familiar with this part please advise.
Thanks
Part Number: DAC60096 Team,
I have a customer with a mistake in their layout and one of the DAC outputs is shorted to AVSS.
In order to eliminate the short they need to drill an AVSS ViA but this will also detach pin F6.
This DAC has 16x AVSS (negative…
Part Number: DAC60096 Hello,
I am currently designing a pcb with DAC60096. I am just curious whether this DAC 60096 is a surface mount or a through hole device. Any clarification on this is highly appreciated. Thanks!
Part Number: DAC60096 Team,
I have a customer designing with DAC60096, and they've run into a discrepancy regarding the VREH/VREFL and AVSS/AVDD pins. Please see questions below:
Data sheet states 100nF cap should be used on page 5, but on the EVM…
Part Number: DAC60096 Tool/software: Code Composer Studio Hello!
I can not understand how to correctly set the parameters PTR for access to the DAC? The first subsystem contains DACs from 1 to 24. The second subsystem contains DACs from 1 to 24. The third…
Part Number: DAC60096 Hi all,
I am facing similar problem with DAC60096. I am using SPI interface designed inbuilt to communicate with DAC60096.
To send data to DAC1-G1:
1. address x18 (PTR), data x00, x00 (total 24 bits), this is for selecting DAC1-G1…
Part Number: DAC60096 Hello,
I am trying to send SPI data from an Aardvark host adapter to the DAC60096. When I use the SDM-USB-DIG to connect from my PC to the DAC, data is sent fine. Additionally, I can see the 16 bit strings necessary to write to the…
Part Number: DAC60096 Hello,
I am trying to communicate with my DAC60096 by sending data from an Aardvark host adapter. I am wondering about the pins on the DAC. There are 8 SPI pins, only 4 of which correspond to output headers on the Aardvark (SCLK…