Hello I have written the following commands to write some voltage over SPI and to get a read out to varify that the sttings went OK. DO i need another "read" command for that purpose?
Thanks.
//start write update command
uint8_t B7_B0…
Part Number: DAC80004 Other Parts Discussed in Thread: MSP430FR2311 , DAC81416 , ENERGIA Tool/software: Code Composer Studio Hello,
I'm trying to evaluate the DAC80004 and connect it to msp430fr2311
I use C to control the DAC80004 but it's no output…
Part Number: DAC80004 Hi,
In my design with DAC80004IPW, the CLR pin is left floating. I don't see the DAC output changes with reference to the programmed DAC input code.
The LDAC pin is tied to ground through a 2K resistor and POR is connected to…
Part Number: DAC80004 Hello, everyone. The confusion is as follows. If we use a 3.0V reference as the full-scale voltage, then 1LSB is about 3/(2^16-1)=46uV. If we want to guarantee the 16bits resolution we should make the total output peak-peak noise…
Part Number: DAC80004 Hello,
I'm trying to evaluate the DAC80004EVM and connect it to RPI3 module to SPI0.
I use python to control the DAC80004 but w/o success.
I'm not using signals CLR~ nor LDAC~
My code below:
import spidev import time import…
Part Number: DAC80004 Hello Guys,
I have similar problem as you had, and you forgot to post the solution. What was the issue in your case?
According to the datasheet, the CLR pin is falling edge sensitive, so keeping it high or low has no difference in…
Part Number: DAC80004 Hello Team,
on page 8 of our datasheet you see a 'Stand-Alone Timing' (Figure 1). There is a timing t19 mentioned which is used in two ways:
- between SDIN and SYNC line
- between CLR and VoutX
Is this correct?
Many Than…
Part Number: DAC80004
Hello again,
I use this routine to set DAC Power on and off
void set_dac_power(uint8_t mode) { dbgMess("DAC Power: %s ! Value= %i",mode == 1 ? "OFF" : "ON", mode); if (mode==1) SPI_send_data(WRITE_DAC…