Other Parts Discussed in Thread: THS5651A Hello E2E,
I was looking through the DAC900TPWRQ1 data sheet on the website and maybe I'm missing it but I can't seem to find information on how much time should be given to the part after coming out of Power Down…
Other Parts Discussed in Thread: DAC900 , THS4281 , LMH6321 , THS4021 , THS4221 Hi
I am Using DAC900 in my design. DAC Clock is 50MHz Max. The output voltage required is 0 to 12V with 300mA maximum current.
The supply voltage available is +/- 12V. Kindly suggest…
Other Parts Discussed in Thread: DAC900 I am using DAC900 in my board. Is there any availability issues with DAC900 for next 15 years.
It will be better if you could suggest any other recent equivalent device to replace DAC900.
DAC clock is 50MHz.
Regards…
Other Parts Discussed in Thread: DAC900 , THS5651A , DAC5652 Hi,
Let me ask you a question about high speed DAC like DAC900/5652, THS5651A.
Q) Response time between “External Reference change” and “IOUT”
In external reference mode…
Andreas,
No. You would have to build an adapter board or a harness to interface to the two different connectors. Both headers used have male pins. Some DAC board options are the DAC900, DAC902, DAC904, DAC908, DAC5652, DAC5662, DAC5672, and DAC5671 EVM…
Part Number: OMAP-L138 Other Parts Discussed in Thread: DAC8734EVM , , DAC900 I am generating a 455 kHz digitized and AM modulated sinewave signal using the DSP, and need to convert it to an analog signal. I plan to use either a serial DAC such as the TI…
Elsa:
You can check out the DAC5652 CMOS dual, 10-bit DAC operating at 275 MSPS or the DAC3151 LVDS single, 10-bit, 500 MSPS DAC or the DAC900 CMOS single, 10-bit, 165 MSPS.
--RJH
Other Parts Discussed in Thread: DAC900 Hi.
I want to understand how to set absolute values of resistor in the circuit of attached file.
(This circuit is on the datasheet P.13 of DAC900) The resistor is R1 and R2 (R3 and R4). The value of Iout is 20mAp-p…
Thanks a lot for the responses.
If I want to connect a ADC/DAC (such as DAC900) to a PC using uPP interface, what would be the best micro-controller or any other chip?
I found out "TMS320F28374S" has uPP interface, is there any other chip as well to do…