Hi Edu,
We checked the DDC264 documents, however, DDC316 has more functionality which is not explained in detailed in DDC264. There is a gudeline on board design for DDC264 but the layout is not as detailed as for DDC316. Since DDC316 is for reading ultra…
Part Number: DDC316 We did some intensive tests with the DDC316 and noticed a signal noise due to Range Error Match (0.2%FSR typ., 1%FRS max.) between side A integrator and side B integrator of the same input.
This meas with RANGE[1:0]=11, max. input…
Part Number: DDC316 Hi,
Which kind of flux is BGA package( DDC316CGXGT ) included?
R (Rosin) RMA (Rosin mildly activated) RA (Rosin activated) WS (Water-soluble)
https://en.wikipedia.org/wiki/Flux_(metallurgy)#Flux_recovery
Best Regards,
Kuramoc…
Part Number: REF6141 Other Parts Discussed in Thread: DDC316 , REF3140 , , OPA350 , REF35 Good afternoon,
In one of my designs I am using a DDC316. In the reference schematic in the datasheet of the DDC316 (p.19 Figure 15), an external reference is supplied…
Part Number: DDC316 Hello,
I am trying to interface DDC316 with FPGA. I am using spartan 3 FPGA board. I have set the clk frequency 40 MHZ and conversion time 20 us. After configuring the configure resistor through Din_CFG pin, Dvalid is still high.
…
Part Number: DDC232 Other Parts Discussed in Thread: DDC264
Hello,
I want to use the DDC232 without an FPGA directly connected to a Piccolo controller. In my application I want to connect a photodiode-array to the chip. The output-current FS-range lies…
Part Number: DDC316 Hi,
I'm testing a DDC316 which has been assembled onto a breakout board. In order to get an indication of the integrity of the connection of the BGA package to the board, I am initially measuring the 'quiescent' analogue and digital…
Part Number: DDC316 Hi,
Really simple question - couldn't quite figure it from the datasheet..
Does the 16bit configuration register have to be set for each conversion cycle or once written to will it remain set for subsequent cycles (as long as it…
Other Parts Discussed in Thread: DDC264 , DDC264EVM , DDC232 , DDC114 , DDC118 , DDC2256A , DDC112 , DDC1128
1. Is the hardware trigger active in the DDC264 evaluation board?
What is the amplitude and shape of the input trigger signal that can be issued into…