Other Parts Discussed in Thread: DDC316 Hello,
where I can find some thermal metrics for DDC316 package like "junction to ambient" or "junction to case"? I have to estimate the junction temperature in my design.
Thank you.
Best Regards…
Other Parts Discussed in Thread: DDC316 , DDC232 Hello,
we currently using a system with DDC316 or DDC232 to measure a proton beam. To improve our results and remove noise pickup we want to move the DDCs into our chambers. Are there any test done on the…
Other Parts Discussed in Thread: DDC316 , ADS1274 , IVC102 On the DDC316, is it possible to many consecutive samples in between consecutive resets? I ask because I would like to perform "up-the-ramp" sampling and essentially line fit my integrated signal…
Adam,
we reconfigure DDC316 in each CONV cycle but after the data read (this way we were configuring DDC316 for the next cycle) and before CONV toggles. This worked before delaying data. We thought that we were satisfying the condition "before CONV toggles…
Other Parts Discussed in Thread: DDC316 Hi,
We`ve began working with a DDC316 converter. The timing/clocking issues are pretty clear, however a communication (data retrieval) example would be greatly appreciated!
Also, we use an earlier version of Orcad…
Other Parts Discussed in Thread: DDC316 Hello,
I am using three DDC316 at one SPI.
After Power on, I can read the first Four Channles of the first DDC316.
If I try to switch the DDC316 in DaisyChain Mode by writing the Configuration Bits, DValid is…
Hi Alex,
Probably DDC232 would be the closest to what you ask, with 32 channels and similar behavior to the DDC118. Cost per channel should be lower too.
The other device would be the DDC316 but it is 16bit "only" and the full-scale range is lower. It…
Other Parts Discussed in Thread: DDC316 Hi,
Just want to get some verification on clocking these DDC316 parts. The spec says system clock min. 1 max. 40MHz and Data clock max 40MHz.
My question is can the data clock be anything below 40MHz or 20MHz when…
Other Parts Discussed in Thread: DDC316 , DDC232 Hello:
I bought several ddc232 and ddc316, I am not using it for ct scan, I only have 16 photodiodes.
I am wondering what kind of adapter should I use for their nfbga 8x8 config.
Or is there a PCB can…
Other Parts Discussed in Thread: DDC2256A , DDC316 , ADC3221 , ADS8168 Hi TI
Is there any digital DDC thip or ADC chip with Integrated DDC for 200K-400Khz using now?