Part Number: MMWCAS-RF-EVM Hello TI Team
I am using MMWCAS-DSP-EVM along with MMWCAS-RF-EVM and capturing the data using Cascade_Configuration_MIMO.lua and Cascade_Capture.lua. Eventually, I want to scan a defined area at different spatial points using…
Part Number: LAUNCHXL-F280025C Other Parts Discussed in Thread: DRV8353RS-EVM , Hi,
Setup is LAUNCHXL-F280025C + DRV8353RS-EVM , running Universal Motor Control Lab.
DMC_LEVEL_1 is set..
Offset_V_sf is 1.0 vs 0.5 expected. Current offset is OK.…
Part Number: UCD3138PFCEVM-026 Hello,
We bought UCD3138PFCEVM and I am trying to test it.
I followed the steps mentioned in the user manuals and connected the PFC Eval to 240Vac input
On the first attempt, I think only the bridge rectifier was…
Other Parts Discussed in Thread: TLV320DAC3100 , PCM1774 , PCM1870A , PCM1870 , TLV320ADC3101 , TLV320ADC3001 hi, i need buy this evaluation boards, but i can not find them.
DEM-DAI1774 EVM
DEM-DAI1870 EVM
I've only found the user guide.
regards…
Part Number: SK-AM62 Other Parts Discussed in Thread: CCSTUDIO , SYSCONFIG , UNIFLASH Hello all,
I have just started using the SK-AM62 EVM board from TI.
I was able to start the board and boot the EVM using SD card as described under link
https…
Part Number: AM2634 Hi Team,
I am trying to download multicore empty project in which I have modified section memory address
Initially sections were pointing to OCRAM but I have changed to Flash. But, when I try to download the code into cores it…
Part Number: DP83TG720EVM-MC Other Parts Discussed in Thread: DP83TG720S-Q1 , USB-2-MDIO Hello Team,
can you confirm if the bridge on the DP83TG720EVM-MC between the DP83TG720S-Q1 and the DP83867ERGZT may work without the MCU programming.
The optimal…
Part Number: AM6442 Dear team,
we burn sbl_ospi and gpio_input_interrupt to flash,then press SW5 on AM64x-evm GP board,gpio interrupt generated successfully as below log:
Key is pressed 1 times
Key is pressed 2 times
Then we burn sbl_ospi_linux…
Part Number: TDA4VM Hello Champs, Customer wants to run the IIC usercase on the TDA4VM EVM platform.The source code path is as follows: pdk_jacinto_08_05_00_36/packages/ti/drv/i2c/example/i2c_utility/i2c_utility_main.c He is using makefile to compile…