Part Number: RUN-FDA-4567-EVM Dear all,
for evaluate the feasability of using the RUN-FDA-4567-EVM evaluation board I'd like to know the following dimensions
the outside dimensions of the board,
the positions of the mounting holes,
the position…
Part Number: AM625 Hey,
I am trying to run sbl keywriter on am62x evm. Unfortunately after few days I am still not able to do it, programmed firmware seems to not running. I've done everything that was written in am62x academy related to this topic…
Part Number: F29H85X-SOM-EVM Hi all,
Customer has a single project which run originally on the CPU1. There are some 64bit variables in the project. So they want to load this project into the CPU3. If customer did not revise this project to the multicore…
Part Number: AUDIO-AM275-EVM Hello Experts,
I am trying to run the example code "GPIO"/"Hello World"/"Audio Loopback" on the AM275-EVM but am facing issues while running the code through JTAG (XDS110) via micro USB. When I hit run, I see this error…
Part Number: AWR2944EVM Other Parts Discussed in Thread: AWR2944 Hello TI Support team,
I am developing a multi-sensor setup using two AWR2944EVM boards and would appreciate your guidance on running them in close proximity.
Concept: I want to mount…
Part Number: MCF8329A Other Parts Discussed in Thread: MCF8329RRYEVM Hello,
I tunned the bldc motor from GUI and saved the tunned parameters as .json formate.
I want to run the motor using GUI and/or individually (without GUI) using EVM board MCF8329RRYEVM…
Dear Alicia,
I was meanwhile successful to run a similar board LDC1101click from MIKROE via an Arduino controller. So I intend to break up the EVM and proceed that way using my own sensing coils now.
I was chosing LDC1101 for its high sample rate…
Part Number: USB-PD-CHG-EVM-01 Other Parts Discussed in Thread: BQ25798 , TPS25751EVM Hi team,
I’m evaluating the USB-PD-CHG-EVM-01 and would like to confirm Source operation, specifically sourcing a 20 V PDO on VBUS.
Is it supported/safe to inject…
Part Number: DEM-OPA-SOT-1A Hi Team, Need your assistance on this minor discrepancy that one of our customer had raised. On the pin configurations pin 5 is /DIS and pin 6 is Vs+. We have noticed that on the DEM-OPA-SOT-1A typical application circuit …