Part Number: AM2434 Tool/software: Dear Texas Instruments Support Team,
We are currently planning to use the AM2434 for an upcoming project and have purchased the corresponding EVM module through Digi-Key.
Using the onboard XDS110 interface, we…
Hi Haseen,
Thanks for testing and sharing your results.
Along with your testing using the bench power supply, we also replaced the buck converter on the EVM board and tested it on our solar setup, which is similar to the field conditions. This new…
Part Number: TPS55289 Tool/software: Hi Guys,
We procured two pcs TPS55289EVM-093 from Mouser and Digi-key respectively.
Both of them are not working.
we use AMD FPGA to drive TPS55289EVM-093. I2C is 100KHz.(Oscilloscope Waveform is shown below…
Hi ,
I tested the same on SDK VERSION 10.01.00.04 and it is working fine on our TI EVM.
Target board logs:
Welcome to minicom 2.8
OPTIONS: I18n
Port /dev/ttyUSB0, 16:11:12
Press CTRL-A Z for help on special keys
U-Boot SPL 2024.04-ti…
Hey Maik,
Does this look right?
EVM User's Guide: DRV8432EVM Motor Drive Evaluation Board
DRV8432EVM User Guide.pdf
If you're driving a brushless (BLDC) motor I highly recommend checking out our BLDC product line instead. The DRV8432 device is…
Part Number: LMG1210EVM-012 Other Parts Discussed in Thread: LMG1210 Tool/software: Hi, I found out that the C-boot is not charging up to 5V at every switching cycle. I'm attaching the scope traces of the HB-HS w.r.t other signals. The board was supplied…
Asha Bhandarkar said: Please check if this is a pathing issue, and report back if that fixes issues.
I have cleared flatbuffer issue.
The make command got executed successfully, but while executing make tidl TARGET_PLATFORM=PC command facing the…
Govindharajen M said: I have read the registers 0x09, 0x00, and 0x01 is show only the value that I have written.
I don't understand what you mean. Are you saying you are reading correctly the values you have written?
The Figure-22 you are showing…
Part Number: F29H85X-SOM-EVM Other Parts Discussed in Thread: AM263P4 Tool/software: Hello,
We would like to develop a motor controller using the F29H859 C2000 F29 processor that can drive two AC motors for traction and one motor for pump applications…