Part Number: DIYAMC-0-EVM Other Parts Discussed in Thread: AMC0230D , Hi TI Team,
I am encountering an issue when using the AMC0230D to measure AC input voltage. I am using the DIYAMC-0-EVM.
Setup Details: A voltage divider consisting of (360kohm…
Part Number: F29H85X-SOM-EVM Other Parts Discussed in Thread: HSEC180ADAPEVM , DP83826E Hardware -------- - Board: F29H85X-SOM-EVM (Rev A, BAW SE oscillator variant — same board reported working by user Trieu To in thread 1574661) + HSEC180ADAPEVM - Device…
Part Number: AWR6843AOPEVM Other Parts Discussed in Thread: AWR6843AOP , UNIFLASH , DCA1000EVM , AWR6843 Hello,
I am trying to capture LVDS data from AWR6843AOP (RevG) using DCA1000 EVM on Ubuntu Linux. DCA1000 FPGA responds to all UDP config commands…
Hi Praveen,
Which method should exactly do i need to follow because i am not able to boot from emmc completely(without help of SD card). here is my u-boot log with emmc partition and files U-Boot SPL 2025.01-g70667128cb5b-dirty (May 02 2026 - 14:44…
Part Number: TPS4810Q1EVM Other Parts Discussed in Thread: TPS4810-Q1
Hi,
I am evaluating the TPS4810-Q1 using the TPS4810Q1EVM board. I am observing unexpected behavior at VOUT when there is no load connected.
Setup:
Board: TPS4810Q1EVM
VIN…
Part Number: USB-PD-CHG-EVM-01 Other Parts Discussed in Thread: BQ25750 , BQ25798 Tool/software: I would like to use the USB-PD-CHG-EVM-01 in a test application for testing mobile charging bricks and other charging devices. I was wondering if the USB…
Part Number: J721EXCPXEVM Hello experts, Here is a full summary of the problems i have while trying to start simple onnx model with vx_app_tidl_cam_test.out from vision_apps:
960fbc28-3ebd-4a7b-b041-9d5eb2b76deb.pdf My config on device look like this…
Hi,
Apologies for the delay here. We've encountered a few setbacks for releasing the models.
For the time being, the device can easily be evaluated with this EVM: https://www.ti.com/tool/DIYAMC-0-EVM
Additionally, are there any particular lab setup…
Part Number: F29H85X-SOM-EVM Hello Experts, I already asked question regarding Frame selection and EPWM16 giving error when working with different Frame and shared with CPU3. What I observed it that when I use Frame 0, EPWM 16 works normally in CPU3,…