Other Parts Discussed in Thread: AM3359 Dear all,
The original ethernet port seems can not work on my AM3359 EVM board.
Sometimes, I can see "phy 0:0 not found" on the console log.
I also tried to use network cable to connect to switch hub, but…
Hi all
I use DVRRDK4.1. In my code, I found a problem.
I add a Vps_printf statement at function System_ipcMsgQCreate() src_bios6/links_common/system/system_ipc_msgq.c , seems the three slave create messageQ queue success:
[c6xdsp ] MessageQ: DSP_MSGQ…
Installing ti-sdk-am335x-evm-05.06.00.00-Linux-x86-Install leaves me with a number of 0 byte files in the root directory, including the setup.sh and Makefile:
-rwxr-xr-x. 1 ken ken 0 Dec 16 14:52 Makefile -rwxr-xr-x. 1 ken ken 0 Jan 14 20:38 Rules.make…
Hi,
I am using the saLoopBack application to capture video at 1280x720p. The format of the captured video is coming "YUV2" ,i.e YUV 4:2:2(16bpp).
But i want the output video as YUV 4:2:0.
Can you please tell what modification I have to do in the…
Other Parts Discussed in Thread: AM3352 Dear all,
I'm using custom board with AM3352. I need to only 3 uarts without cpld and lcd. (used profile 0) Just like baseboard type of AM335x GP EVM.
I modified some code below.
\linux-3.2.0-psp05.06.00.00…
Other Parts Discussed in Thread: SYSCONFIG Hi everyone,
I'm working on a project where I've just purchased an OMAP-L138 EVM from Logic PD and gone through the test programs, which seems to be working fine. But to continue with my project I need to be…
“Zero cells found” could also mean,
– One of the PowerLAN nodes is not working.
– The Expected Number of Cells does not equal Actual number found.
Use iterative approach of loading .tmap files until you can no longer build a PowerLAN Network. This…
Hi there,
I'm trying to load the following source code at address 0 of a DM6446 EVM (portion of the listing file shown below)
9 00000000 E59FF018 ldr pc, addr_onReset 10 00000004 E59FF018 ldr pc, addr_onUndefined 11 00000008 E59FF018 ldr pc, addr_onSWI…
Other Parts Discussed in Thread: CDCE62005 , CDCE62005EVM I am using CDCE62005 Control GUI to test out my settings on an CDCE62005evm board trying to solve a lock issue. Whenever I load my settings I see them applied for a second, then register 0 gets…