Hi Alark,
The application note is targeted for 'Augmented HUD", this type of HUD creates a virtual image in front of the car in the line of site.
I guess by simple HUD you mean either a projector HUD or Teleprompter HUD. These two type are relatively…
Other Parts Discussed in Thread: DLP9500 , DLPLCRC410EVM Short description: DLP using for high speed video simulation Case details or comments:
We need to create video simulator on base DLPLCRC410EVM and DLP9500 0.95 module. We need to generate video…
Hi Amelie,
Thank you and your customer for considering the use of our DLPC120-Q1 and DLP3030-Q1 chipset. No, we do not have an integrated DLP LED driver. Careful selection of components and a good circuit layout will help thermal performance and improve…
Part Number: DLP5530-Q1 Other Parts Discussed in Thread: DLP5534-Q1 , , DLP5531-Q1 Hi DLP Experts, We need your assistance on this as our customer needs more information before choosing their DMD. We have studied the datasheets of DLP5534-Q1, DLP5531-Q1,DLP5530…
Part Number: DLP3030-Q1 Other Parts Discussed in Thread: DLP3030PGUQ1EVM Please tell me about the image generation unit(DLP 3030 - Q1).
Question 1: Can this product be projected from the PC as it is with HDMI input? Question 2: Is it possible to project…
Part Number: CC2652R Other Parts Discussed in Thread: RF-RANGE-ESTIMATOR , ZIGBEE-POWER-CALC , Z-STACK , SIMPLELINK-CC13X2-26X2-SDK Hi,
Application: Animal individualized monitoring
Background: The detection of individual animal including temperature, motion…
Hi Sudha,
Welcome to DLP forum and thank you for your interest in DLP technology. Could you please share more details about your application and how you intend to use DLP2010 Lightcrafter EVM? www.ti.com/.../DLPDLCR2010EVM
The EVM comes with drive…
Renan
DLP DMDs are fabricated in our high volume semiconductor process. It would be incredibly expensive to build custom variations. As Fizix asked above if you can provide more details as to the application and possible volumes we could look at building…
Hi Pratik,
Welcome to DLP forum and thank you for your interest in DLP technology.
Did you use the "optical Module Search Tool" in the following page:
www.ti.com/.../DLP-OMM-SEARCH
Please select engine which meets your requirement and also…
Dear Abraham
EKB Technologies offers IR Laser version for 3010-LC called IR E3010-LC with high depth of focus specifically for volume measurement embedded applications.
For additional details please see our eStore at: www.ekbtechnologies.com/.../dlp-lightcrafter…