Hello Eric,
After further looking at the question I do not believe this ripple should be a concern as those voltages are within the minimum and maximum limits.
I am closing this thread due to inactivity. If the customer has further questions or issues…
Part Number: DLP230NP Dear,
Hi,
Could you please let me know how to run init_parallel_mode.py to display an image? The image is in Raspberry Pi, so I just need the projector to recognize it and then display it. I have initialized communication between…
Part Number: DLP230NP We have a explanation for the rotation angle of DMD active array on the datasheet.
---ROTATION ANGLE OF DMD ACTIVE ARRAY IS A REFINEMENT OF THE LOCATION TOLERANCE AND HAS A MAXIMUM ALLOWED VALUE OF 0.6 DEGREES.
My customer want…
Part Number: DLP230NP Hi
We looked with a microscope and found that there were slight scratches and white spots on the exterior. Could you please help me confirm whether it affects the use? What is the cause of this?
Thank you
Part Number: DLP230NP When we recently used the DLP230NP, more than 2% of the DMDs randomly appeared bright pixels, which were not on the BBF lines. Is there a better direction for investigation?
In addition,this batch of DMD has been stored for 2 years, and of course it was stored according to s…
Part Number: DLP230NPDLP230NP .23 1080P DMD we use so far in factory, that DMD has blemish happened after this some DMD units was clearing, that blemish is still happened.
May I know this DMD spec? about blemish issue.
I use gray10 or blue60 pattern…
Part Number: DLP230NP Hi Experts,
DLP230NP .23 1080P DMD datasheet (Rev. C) (ti.com)
The above link is the datasheet. On the page 24,
"The conversion constant CL2W is based on the DMD micromirror array characteristics. It assumes a spectral efficiency…
Part Number: DLP230NP Other Parts Discussed in Thread: DLP230GP , DLP160CP , DLP2010
We are connecting a pico projector to a smartwatch mother board and need all information helpful including 3D files of parts preferably for 3DS max. We have patented a…
Part Number: DLP230NP Hi Team,
Can you please check and advise with following request?
"
Within the scope of the study, an optical analysis setup must be set up.
We cannot open the attached file on the Texas Instrument site in Zemax 2013 (student…