Part Number: DLP3010EVM-LC Other Parts Discussed in Thread: DLP4710EVM-LC Dear engineer, hello!
I have a question for you!I used DLP3010EVM-LC to do Splash Patterns test.My Settings are as shown in picture 1.I used image 4 for the projection. The result…
Part Number: DLP3010EVM-LC Other Parts Discussed in Thread: DLP3010
Hi Team,
Our customer is looking for the dimension of the DMD housing in DLP3010EVM-LC evaluation module. Please see the details of his inquiry below.
We're using DLP3010 EVM LC. For…
Part Number: DLP3010EVM-LC Hi Team,
Customer is trying to display a series of Gray Patterns which consists of 20 horizontal patterns and 22 vertical patterns. They loaded the patterns into the DLP, then they tried to display the patterns with “Run Continuously…
Part Number: DLP3010EVM-LC This is with respect to the flex cable of DLP3010EVMLC. If the flex cable is to be folded, will it affect the signal quality or any other parameter required for sending accurate signals to the DMD?
Part Number: DLP3010EVM-LC Other Parts Discussed in Thread: DLPC3478 , DLPDLC-GUI Hello.
I am now looking for a way to set the LED start current.
The default current set on the DLPC3478 is 1500mA, which is too high for my purposes.
I updated the firmware…
Part Number: DLP3010EVM-LC My experiment required the DMD to be illuminated by a laser, so I removed the DMD of the DLP3010EVM-LC, which is the DLP3010LCFQK, and placed it on the fixed device (this has a similar structure to the original position of the…
Part Number: DLP3010EVM-LC Other Parts Discussed in Thread: DLPC3478 Hello,
I'm trying to display mp4 videos with matlab with the DLP. I have an issue regarding bit depth. It seems that when setting the bit depth to 1, intensities of the pixel are a bit…
Part Number: DLP3010EVM-LC Other Parts Discussed in Thread: DLP3010 , DLPC3478 , DLPC3430 I am attempting to flash an image onto the DLP3010, however I am unable to communicate with the board. I am using "DLP EVM GUI" to interface with the board. The board…
Part Number: DLP3010EVM-LC Other Parts Discussed in Thread: DLP3010LC Hi Team,
Would you kindly help with the question below?
A customer has opened the DLP3010LC EVM and extracted the DMD. They happened to notice that all the light was focused onto a particular…
Hello Mark,
1.) There has been strange behavior when updating on EVM while it was projecting. A more sure fire way to update is to have the EVM connected to power and the switch in the off position (not displaying).
2.) There is an advanced mode in the…