Part Number: DLP5531-Q1 Hi
I am working with DLP-5531-Q1 and would like to send a custom image to the DLP which seems to require access to DLP-AUTO-HEADLIGHT-GEN2-EMBED-SW-CONFIG-FILES – DLP Auto Headlight Gen 2 - DLPC230 Embedded Software and Configuration…
Part Number: DLP5531A-Q1 Hi TI Team,
I am currently using the DLP5531-Q1. When I input an image with a resolution of 1902x1521, the black-and-white line pairs in the output image appear blurry and are not clearly resolved.
Could you please explain…
Part Number: DLP5531-Q1 Other Parts Discussed in Thread: DLPC230-Q1 Tool/software: Dear,
How to download DLPC230-Q1 Control Program. I need the software to Control DLP5531-Q1 Electronics Evaluation Module
Part Number: DLP5531-Q1 Other Parts Discussed in Thread: DLP5531LEQ1EVM Hi,
we purchased a DLP5531-Q1 evaluation kit. we flashed the firmware and get this error when we start up the system. We connected the system as per the instructions. What could…
Chris,
For the DLP5531-Q1, did you find this download file which has more updated system mounting information. https://www.ti.com/tool/download/DLPR072
This is located in the design and simulation for the DLP5531-Q1. Let me know if this is what…
Part Number: DLP5531-Q1
I downloaded the Altium footprint of DLP5531(CPGA149_FYK_TEX) from TI and used it to make a PCB Board.
Then I found the PCB board could not match with DLP5531-Q1.
The length of DLP5531 in the datasheet is different from what…
Part Number: DLP5531-Q1
Hi, following up on this thread [e2e.ti.com/.../4031155, I have been continuing with our work on the DLP. We are still facing some issues and would like to seek additional assistance before being able to work on this component…
Part Number: DLP5531-Q1 Dear specialists!
We are developing now an illumination system using Texas Instruments's model DLP5531.
And we have a pair of questions.
1. Do we understand right that for incident spot angular divergence in transversal direction…
Part Number: DLP5531-Q1 Hi I want to know which chip should I use among 5530-Q1,5531-Q1 and 5534-Q1, if I want to illuminated the DMD chip only with green wavelength and 10 W optical power, and use full resolution of 1152x1152 video.
Part Number: DLP5531-Q1 I am considering the use of DLP in an application where it will be exposed from 101kPa to 10kPa.
Is there any altitude and/or decompression data data available for DLP5531-Q1 (or any other DLPs)?
Thanks in advance.