Part Number: DLP650LNIR What's the damage threshold of the product of DLP650LNIR When it's used for the laser pulse of 800nm, 35fs,1KHZ? Can the damage threshold reach 0.1GW/cm2? If this product can't afford this power density, is there any other DMD…
Part Number: DLP650LNIR Customer is considering DLP650LNIR NIR DMD and is concerned with damaging the device. Laser specifications below:
Ti:Sapphire laser – no amplifier. 800 nm wavelength Pavg = 1 W, Pp = 125 kW uniformly distributed over chip Peak…
Part Number: DLP650LNIR Other Parts Discussed in Thread: DLPLCRC410EVM Hi
I have a DLP650LNIR + DLPLCRC410EVM evaluation module which has been running with no problems when connected to a Windows 7 laptop, used for development.
Now I need to use a Windows…
Part Number: DLP650LNIR Good day.
I wonder is it possible to oscillate DMD micromirrors with constant frequency, f.e. 100-5000 Hz. and is it possible to change the oscillating frequency manually? I mean is it possible to make a bit simpler device with…
Part Number: DLP650LNIR Other Parts Discussed in Thread: DLP4500NIR , DLPC350 Hi Team, Our customer is considering to use the DLP650LNIR in the 2500nm wavelength. They are aware that the DMD was only specified at 2000nm and would like to simulate the transmission…
Part Number: DLP650LNIR Hi there,
We need a data sheet showing the accuracy of either the individual mirror or the entire mirror array. That is to say, we need the uncertainty in micromirror pitch size (10.8 um) or the mirror active array width (13.824…
Part Number: DLP650LNIR I bought a DLP Discovery 4100 and a DLP 650NIR. I use Texas Instruments software to display binary pictures on DMD. I want to know how to display gray image on DMD.
Part Number: DLP4710 Other Parts Discussed in Thread: DLP2010NIR , DLP650LNIR , DLP4500NIR I'd like to use a DLP for a mid-far IR spectrometer. Can someone please provide the spectral reflectance of the DLP itself, without cover slip or other intervening…