The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.
Too bad. But thanks for the answer.
One would think that if TI hired Elephant to design the Optical Engine, they would now own the design...
I'll take my chances designing an AXT534124 flex expender accounting for the LVDS pins. It should be easier…
Part Number: DLPC3430 Other Parts Discussed in Thread: DLPA2005 , DLPA2000 I am designing board of DLPC3430 + DLPA2000 projection system , and i using the firmware of DLPC3435 _3.0.0_Firmware.img.
I want to modify the splash image by using the DLP LightCrafter…
Part Number: DLPDLCR2010EVM
Hello,
I plan on designing a pico projector using the DLPC3430, DLPA2005, and DLP2010 chipset. Can you please send the updated firmware for these chips to me?
Thanks.
Part Number: DLPC3430 Other Parts Discussed in Thread: DLPA3000 Hi there—I have two questions with regard to the following statement in section 7.3.3.2 of the datasheet: "SPI0_CLK, SPI0_DOUT, and SPI0_CSZ0 I/O can be tri-stated by holding RESETZ in a…
Hello User,
How do you change the display brightness to maximum (from what value to what value)? Do you change the RGB LED current to achieve the display brightness?
Can you still have communicate with the DLPC3430 when the display freezes?
Regards,
…
Part Number: DLPDLCR2010EVM Hello,
I am looking to create a new PCB to use with the DLPC3430, DLPA2005, and DLP2010.
Instead of using the HDMI input like the evaluation kit, I would like to use displayport.
I have identified this chip for converting…
Part Number: DLPC3430 Hello,
I have a design which uses the DLPC3430 and it receives pixel data over the DSI interface. Under normal operation (both host DSI processor and DLP are operating) the output is fine.
The issue occurs when the host processor…
Part Number: DLPC3430 We are surveying to use DLPC3430 in our customer's product.
There is only one line description on datasheet says the latency is 1 frame.
Some questions we want to know but not much information on data sheet.
Listed below
1.What…
Part Number: DLPC3430 Other Parts Discussed in Thread: DLPC3435 , DLPC3438 , DLPC3433 , DLPC3432 Good Day,
Is there any I2C command to switch between DSI Input and Parallel Input for DLPC3430?
I do not find the command in "DLPC3430, DLPC3432, DLPC3433…
Part Number: DLPC3430 Hi,
In the datasheet for the DLPC3430, in Table 1, (Seen below) the I/O definition is defined as B_10
.
If you look at the Table 3, I/O Type Subscript Definition, subscript 10 is not present.
Where can I find documentation for…