Part Number: DLPC350 Hi Team,
We would like to ask your help regarding our customer's inquiry below.
I have the PRO4500 optical engine from Wintech which has the DLPC350 driver board. Currently, I am using the LightCrafter4500 application to display…
Part Number: DLPC350 Hi TI,
Our own designed DLPC350 control board sometimes does not respond to USB read commands wthin 3sec or more.
This usually happens when sending USB read command 0x1A0A (Hardware Status) or 0x1A1A (Validate Data Command Response…
Part Number: DLPC350 Hi Austin,Akhil or TI expert
I have another question about "I2C_BUSY GPIO". Please answer each question.
(1) Does this signal change for all commands? Ans → (2) Do you know the minimum and maximum busy time? Ans → …
Part Number: DLPC350 Hi Mayank,or TI expert
I have a question about I2C access of DLPC350.
Currently, DLPC350 firmware fair Ver1.1 We are operating the equipment used.
However, there is an I2C hang problem Change to firmware Ver4.1 or 4.4 I'm trying to solve…
Part Number: DLPC350 Hi Experts,
Good day. Seeking assistance on this query:
Where can I get the dlpc350 api develop document? We're using the product. In my program, I can't Play twice Sequence , it just can Play once,
Usually step is : first…
Part Number: DLPC350 Dear TI-er
My customer have a issue because of the area .
Q1) what's the problem 1.2V Core, I/O, FPD at the same time Q2) 2.5V power whthout the timing ? Q3) Termination resistor is 50ohm in the datasheet. Can I use 22ohm ?
DLPC350ZFF…
Hello, E2E support. Good news, Software crush issue already be fixed it, but I found another questions. The DLP devices will get wrong GPIO number some time. We defined MAX_GPIO = 8 and using 4 DLP devices, Question 1: Is the one pin equal to one DLP device…
Part Number: DLPC350
Thank you for your reply. I have written the question in English, so please answer.
I made a DLP control board using DLPC350. The basic design is based on Ti's Lightcrafter schematic.
There was a problem that USB did not recognize…
Part Number: DLPC350 Dear Sir or Madam,
we currently use the S29GL064N90TFI01 as flash for the DLPC350 in our design.
This flash is discontinued by the manufacturer. Our distributor gave us the S29GL064S70TFI010 as an alternative.
Because it has slightly…