Hello Brutus,
You should be able to get the EVM firmware version on the Information page if you are using DLPDLC-GUI .
Do you only see the issue with internal pattern mode?
Regards,
Lori
Hello User,
These questions depend on how you want to design your custom board. TI provides the reference design ( TIDA-080003 ) for DLP3010EVM-LC . Please see the answers below for reference:
1. DLPU074A – section 3: For DLP3010EVM-LC, you need to download…
Part Number: DLP4710EVM-LC Other Parts Discussed in Thread: DLPDLC-GUI Hi there,
Can I have an image file that disable the LEDs on booting sequence?
I'd like to disable LEDs when I press the power switch and turn on/off the LEDs later.
Or if I can…
Part Number: DLPC1438 Other Parts Discussed in Thread: DLPA2005 , DLP301S , DLPDLC-GUI Hello.
I designed a custom board, DLPA2005 + DLPC1438 + DLP301S with flash memory AT25SL321(1.8V, Dialog Semiconductor) which is compatible with Winbond W25Q32.
What…
Hello Jack,
Welcome to the E2E forum and thank you for your interest in DLP® technology!
The DLPDLC-GUI is recommended if a non-EVM firmware image is being flashed onto the system. This Light Control GUI is more agnostic as to which system is being…
Hello Alex,
In the default DLPC3479 firmware, the startup operating mode is in Splash pattern with default startup LED current. If you want to change the default startup settings, then you will need to modify the firmware and reflash the EVM with the custom…
Part Number: DLPC3430 Other Parts Discussed in Thread: DLPDLC-GUI , DLP4710EVM-LC
Corrupted flash images can occur when a flash process through the GUI is interrupted or otherwise fails. An attempt to re-flash a DLP Pico EVM or system. The following process…
Part Number: DLPC7540EVM Other Parts Discussed in Thread: DLPDLC-GUI , , DLP471TEEVM Hi Team, Can we ask for your assistance in locating the firmware for DLPC7540EVM? On its product page the only software collateral available is the DLPDLC-GUI. The firmware…
Hello Shyam,
Welcome back to the E2E forum and thank you for your interest in DLP® technology!
If your custom design is based on the DLP4710EVM-LC design, you should be able to use DLPDLC-GUI to flash the firmware with the latest available firmware…